This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Timer_A 定时中断问题

Expert 2115 points


Timer_A_initUpModeParam param = {0};
param.clockSource = TIMER_A_CLOCKSOURCE_ACLK;
param.clockSourceDivider = TIMER_A_CLOCKSOURCE_DIVIDER_1;
param.timerPeriod = 328;
param.timerInterruptEnable_TAIE = TIMER_A_TAIE_INTERRUPT_DISABLE;
param.captureCompareInterruptEnable_CCR0_CCIE = TIMER_A_CCIE_CCR0_INTERRUPT_ENABLE;
param.timerClear = TIMER_A_DO_CLEAR;
param.startTimer = true;
Timer_A_initUpMode(TIMER_A0_BASE, &param);

Timer_A初始化程序如上所示,在中断函数中反转某个I/O,用示波器观察,方波的频率和占空比都在变化,这是为什么?如果将param.timerPeriod 的值增大,例如param.timerPeriod = 3277,则得到的方波频率和占空比都不会变化,param.timerPeriod是写入TAxCCR0寄存器,应该没有最小限制值得说法吧,ACLK=32768Hz