This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于MSP430G2553 串口无法接受问题 请大家帮忙看一下



首先  我用的 是官方的例程    并且板子上有关于RXD  和TXD的跳线帽也已经改成了HW模式    但是进不了串口中断啊   也并不是所有的时候都进不去 可能有某一次收发就挺正常的  我以为是板子和电脑或者串口软件  的问题 可是在我换了一个板子和电脑还有串口软件 时候 还是这样 实在不知道是怎么回事了 求各位帮帮忙呀  有可能是哪里的问题啊  拜谢!!!下面是官方的代码

//******************************************************************************
//   MSP430G2xx3 Demo - USCI_A0, Ultra-Low Pwr UART 9600 String, 32kHz ACLK
//
//   Description: This program demonstrates a full-duplex 9600-baud UART using
//   USCI_A0 and a 32kHz crystal.  The program will wait in LPM3, and will
//   respond to a received 'u' character using 8N1 protocol. The response will
//   be the string 'Hello World'.
//   ACLK = BRCLK = LFXT1 = 32768Hz, MCLK = SMCLK = DCO ~1.2MHz
//   Baud rate divider with 32768Hz XTAL @9600 = 32768Hz/9600 = 3.41
//* An external watch crystal is required on XIN XOUT for ACLK *//
//
//                MSP430G2xx3
//             -----------------
//         /|\|              XIN|-
//          | |                 | 32kHz
//          --|RST          XOUT|-
//            |                 |
//            |     P1.2/UCA0TXD|------------>
//            |                 | 9600 - 8N1
//            |     P1.1/UCA0RXD|<------------
//
//   D. Dang
//   Texas Instruments Inc.
//   February 2011
//   Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10
//******************************************************************************
#include <msp430.h>

const char string1[] = { "Hello World\r\n" };
unsigned int i;

int main(void)
{
  WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
  P1DIR = 0xFF;                             // All P1.x outputs
  P1OUT = 0;                                // All P1.x reset
  P2DIR = 0xFF;                             // All P2.x outputs
  P2OUT = 0;                                // All P2.x reset
  P1SEL = BIT1 + BIT2 ;                     // P1.1 = RXD, P1.2=TXD
  P1SEL2 = BIT1 + BIT2 ;                     // P1.1 = RXD, P1.2=TXD
  P3DIR = 0xFF;                             // All P3.x outputs
  P3OUT = 0;                                // All P3.x reset  
  UCA0CTL1 |= UCSSEL_1;                     // CLK = ACLK
  UCA0BR0 = 0x03;                           // 32kHz/9600 = 3.41
  UCA0BR1 = 0x00;                           //
  UCA0MCTL = UCBRS1 + UCBRS0;               // Modulation UCBRSx = 3
  UCA0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**
  IE2 |= UCA0RXIE;                          // Enable USCI_A0 RX interrupt
  __bis_SR_register(LPM3_bits + GIE);       // Enter LPM3 w/ int until Byte RXed
}

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCIAB0TX_VECTOR
__interrupt void USCI0TX_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCIAB0TX_VECTOR))) USCI0TX_ISR (void)
#else
#error Compiler not supported!
#endif
{
  UCA0TXBUF = string1[i++];                 // TX next character

  if (i == sizeof string1 - 1)              // TX over?
    IE2 &= ~UCA0TXIE;                       // Disable USCI_A0 TX interrupt
}

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCIAB0RX_VECTOR
__interrupt void USCI0RX_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCIAB0RX_VECTOR))) USCI0RX_ISR (void)
#else
#error Compiler not supported!
#endif
{
  if (UCA0RXBUF == 'u')                     // 'u' received?
  {
    i = 0;
    P1OUT ^= 0x01;     
    IE2 |= UCA0TXIE;                        // Enable USCI_A0 TX interrupt
    UCA0TXBUF = string1[i++];
  }
}