This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LFXTOFFG置位的问题

Other Parts Discussed in Thread: MSP430FR5969

大家好!我用的是MSP430FR5969,目前遇到一个问题:

do {
CSCTL5 &= ~LFXTOFFG; // Clear XT1 fault flag
SFRIFG1 &= ~OFIFG;
} while (SFRIFG1 & OFIFG); // Test oscillator fault flag

程序到这里过不了,查看寄存器发现LFXTOFFG=1;注释这段代码后,能正常运行,请问什么原因?

  • 建议测量一下,看XT1 正常起振了吗?


  • Chao Chen17 说:

    大家好!我用的是MSP430FR5969,目前遇到一个问题:

    do {
    CSCTL5 &= ~LFXTOFFG; // Clear XT1 fault flag
    SFRIFG1 &= ~OFIFG;
    } while (SFRIFG1 & OFIFG); // Test oscillator fault flag

    程序到这里过不了,查看寄存器发现LFXTOFFG=1;注释这段代码后,能正常运行,请问什么原因?

    这段代码是检测外部晶振是否工作正常。

  • 我和楼主遇到了同样的问题芯片是FR6972,LFXTOFFG一直显示外接的32768Hz晶振有故障,通过示波器可以看到外部晶振正常起振,而且在XIN上也可以清楚看到晶振的信号。

  • 换一个试试,另外是不是跟晶振配合的电容有问题?官方推荐的是10PF
    参考
    www.ti.com.cn/.../tidrux6.pdf
  • 建议查看下32768Hz晶振的手册,不同厂家和型号的晶振,负载电容有可能是不同的,负载电容的参数在晶振的数据手册里会有说明

  • 你好!我采用的是爱普生公司的实时时钟芯片,内置的32768Hz的晶振,芯片手册上要求VDD上至少有0.1u的电容,这些要求都达到了。现在不是晶振不起振,而是起振后仍然报错,我想问下LFXTIFG报错的逻辑是怎样的,因为确实从波形上看不出任何问题了

  • 是什么报错?是单片机报错?你也采用的这个单片机??你用时钟芯片给单片机提供时钟?

  • 你是怎么观察报错的?

    你在这段代码后写个点量led的代码,然后复位硬件看能不能点亮led

  • 我就是通过LED进行判断,时钟初始化后再循环里一直检查LFXTIFG。现在仍然是初始化无法复位,用信号源给MCU32768Hz,3v的信号可以正常工作,奇怪的很

  • 这个时钟芯片包含了一个晶振,在FOE高点平时可以输出32768Hz的信号,报错是CS中的LFXTIFG报错,报错的同时无法软件复位,查阅手册说这种情况应该是故障仍然存在,但是示波器显示信号是没有问题的
  • 你自己做的板子吗?还是官网的开发板?

  • 自己做的板子,设计的时候已经尽力将靠近MCU了,4层板上下敷铜