This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6989无法降低功耗



单板状况:

MSP4306989一个、复位电路(RC复位:100千欧,0.1uf)、3.0供电;单板上在无其他器件;

1)使用ti提供的低功耗测试程序:msp430fr69xx_lpm3_02.c,ACLK 使用vlo:10KHz,MCLK 1MHz、SMCLK 1MHz;LPM3;

2)烧进单板功耗为8.24mA,使用fluke万用表测得,无法降低功耗;功耗应该为在2uA左右吧;为何会有8mA的电流也搞不清楚原因了。

3)测试程序也比较简单如下所示:

4)参考文章:www.deyisupport.com/.../467.msp430.aspx,

#include <msp430.h>

int main(void)
{
WDTCTL = WDTPW | WDTTMSEL | WDTSSEL_2 | WDTIS_5; // VLOCLK, ~1s interrupts
SFRIE1 |= WDTIE; // Enable WDT interrupt

// Configure GPIO
P1OUT = 0;
P1DIR = 0xFF;

P2OUT = 0;
P2DIR = 0xFF;

P3OUT = 0;
P3DIR = 0xFF;

P4OUT = 0;
P4DIR = 0xFF;

P5OUT = 0;
P5DIR = 0xFF;

P6OUT = 0;
P6DIR = 0xFF;

P7OUT = 0;
P7DIR = 0xFF;

P8OUT = 0;
P8DIR = 0xFF;

P9OUT = 0;
P9DIR = 0xFF;

P10OUT = 0;
P10DIR = 0xFF;

PJOUT = 0;
PJDIR = 0xFFFF;

// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;

// Clock System Setup
CSCTL0_H = CSKEY >> 8; // Unlock CS registers
CSCTL1 = DCOFSEL_0; // Set DCO to 1 MHz
CSCTL2 = SELM__DCOCLK | SELS__DCOCLK | SELA__VLOCLK;
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers to 1
CSCTL4 = LFXTOFF | HFXTOFF;
CSCTL0_H = 0; // Lock CS registers

P1DIR |= BIT0; // Turn on LED

__bis_SR_register(LPM3_bits | GIE);
__no_operation(); // For debugger
}

// Watchdog Timer interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=WDT_VECTOR
__interrupt void WDT_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(WDT_VECTOR))) WDT_ISR (void)
#else
#error Compiler not supported!
#endif
{
P1OUT ^= BIT0; // Toggle P1.0 (LED)
}