This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有一个新的项目想考路用430的MCU,咨询一下MSP430的几种模式:睡眠模式,掉电模式,省电模式,等等这几种Mode的区别。
常用的模式有
Active :运行模式,所有时钟有效,功耗从几十uA到几mA(速度不同,功耗不同)
LPM0 :关掉MCLK,及CPU内核停止运行,但外设有效,比如Timer,串口等等,功耗在几十uA
LPM3: 关掉MCLK,SMCLK,保持ACLK有效,是常用低功耗模式,功耗在几uA,低频时钟有效,Timer,RTC还可以工作
LPM4:关掉所有时钟,可以外部中断(GPIO,SPI,I2C等)唤醒,功耗<1uA
以上提供的是典型值,不同的MSP430系列有不同的数据和低功耗模式,请参考相应型号的datasheet