This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

430单片机可控制外设的功耗要求



430单片机应用于低功耗领域,那么它对所控制的外设功耗有没有什么要求,处理器通过软件控制使其进入低功耗模式,外设如果需要的功耗较大,用430处理器来实现是否可行?

  • 功耗低,意味着驱动电流小,驱动能力也会差,直接去控制大功率的器件会有难度。而且大功率的器件对430干扰也会比较严重。

    个人感觉430适合应用在一些电池供电的便携式设备中。大功率的场合,可以考虑C2000系列。

  • MSP430 IO口的最大驱动能力大约10+mA。一般不会把MSP430的IO口直接拿来当电源用,但是驱动一些LED,以及功耗不太大的OPA,comparator,逻辑器件等等是可以的。

    如果只是去控制外部大功率器件,系统设计时注意把大功率器件的干扰控制好,也是可行的。