This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430x4xx 低功耗晶振的配置



MSP430x4xx 系列单片机在上电时32K 的晶振不能可靠起振?

  • MSP430x4xx 系列单片机集成了软件可编程的输入电容C(XIN)和输出电容C(XOUT),以提供石英晶体振荡器振荡所需的负载电容。在上电时,默认的负载电容为0pF(即没有负载电容)。为了使32KHz 晶体正常启动,必须用软件配置好所需的负载电容。

    实例:对于手表晶振,需要10 到12pf 的负载电容,所以在初始化代码中需要配置XCAPxPF 为18pf切换负载电容时,等待晶振起振和FLL 稳定需要确保有足够的时间。有一个监测振荡器的正常运作与否的方法就是检查振荡器故障位。请参阅数据手册和MSP430x4xx 用户手册关于时序要求,振荡器故障位和XCAPxPF 配置章节。