This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

依次采样模式

ADC10CTL1 = CONSEQ_1 + ADC10SSEL_0 + ADC10DIV_3 + SHS_0 + INCH_11;
__delay_cycles(30000);
ADC10CTL0 |= ENC;
}
/******************************************************************************************************
* 名 称:ADC10_ISR_HOOK
* 功 能:ADC转换完成后唤醒CPU
* 入口参数:无
* 出口参数:无
* 说 明:直接从CCS的Example中移植过来
* 范 例:无
******************************************************************************************************/
#pragma vector=ADC10_VECTOR
__interrupt void ADC10_ISR_HOOK(void)
{
static int inch=0;
o[inch]=ADC10MEM;
inch++;
if(inch>11)inch=0;
//temp =ADC10MEM;
_bic_SR_register_on_exit(LPM4_bits);
}

错误在哪应该怎么写