可以用一块msp430驱动另一块msp430吗?A控制B的上电和断电。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
跟这篇帖子的意思类似。请查看。
MSP430的功耗非常低,而IO的输出能力也不弱,一般都在5mA,完全可以驱动另外一个MSP430工作。
而且也可以多个IO一起驱动,最大提供48mA电流能力。