This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430FR6972 高低速采样的值不一样



我用600HZ去采电压,和用4KHZ去采,采样值能差个2%。不管我把
ADC12CTL0 = ADC12SHT0_1这个采样保持的时间设置多长以及系统低功耗还是去掉ADC12PWRMD,结果都不变?

再问一个问题

1.我现在用的是多通道采样,没用重复的多通道采样。因为我发现用了重复的多通道采样后(并去掉ADC12MSC)。

 

TA0CCR0 = 7; //4; //7; // TA0 4K 采样频率

TA0CCR1 = 3;

本是4KHZ的,结果只有800HZ。为啥?

 

void adcRestart (void)
{

//Turn OFF ADC12B Module & Clear Interrupt Registers
ADC12CTL0 &= ~ADC12ENC;
ADC12CTL0 &= ~(ADC12ON + ADC12SC);

__delay_cycles (10);
ADC12IER0 &= 0x0000; //Reset ALL interrupt enables
ADC12IER1 &= 0x0000;
ADC12IER2 &= 0x0000;
ADC12IFGR0 &= 0x0000; //Reset ALL interrupt flags
ADC12IFGR1 &= 0x0000;
ADC12IFGR2 &= 0x0000;


ADC12CTL0 = ADC12SHT0_1 | ADC12ON | ADC12MSC;

/*用了ADC12OSC(ADC12内部时钟源)分频为1 */
ADC12CTL1 = ADC12SHP | ADC12SHS_1 | ADC12_B_SEQOFCHANNELS; // Use sampling timer 序列通道单次转换

ADC12CTL2 |= ADC12RES_2 | ADC12PWRMD; // 12-bit conversion results //低功耗

#if ADC_INNER_REF2_5 == 1
/*内部参考 */
// Channel2 ADC input select; Vref=VREF buffered
ADC12MCTL0 = ADC12VRSEL_1 | ADC12INCH_2;
ADC12MCTL1 = ADC12VRSEL_1 | ADC12INCH_12;
ADC12MCTL2 = ADC12VRSEL_1 | ADC12INCH_15;
ADC12MCTL3 = ADC12VRSEL_1 | ADC12INCH_13;
ADC12MCTL4 = ADC12VRSEL_1 | ADC12INCH_14 | ADC12EOS;
#else
/*外部参考 */
// Channel2 ADC input select; Vref=VREF buffered

ADC12MCTL0 = ADC12VRSEL_14 | ADC12INCH_2;
ADC12MCTL1 = ADC12VRSEL_14 | ADC12INCH_12;
ADC12MCTL2 = ADC12VRSEL_14 | ADC12INCH_15;
ADC12MCTL3 = ADC12VRSEL_14 | ADC12INCH_13;
ADC12MCTL4 = ADC12VRSEL_14 | ADC12INCH_14 | ADC12EOS;

#endif

ADC12IER0 = ADC12IE4;
ADC12IER2 = ADC12TOVIE | ADC12OVIE;

if (SYSTEM_WORK_MODE_HIGH_ADC == g_systemWorkMode)
{
TA0CCR0 = 7; //4; //7; // TA0 4K 采样频率

TA0CCR1 = 3;
}
else
{

TA0CCR0 = 54; //600HZ
TA0CCR1 = 50;
}

TA0CCTL1 |= OUTMOD_2; // TBCCR0 toggle (ON period = ~230us)

ADC12CTL0 |= ADC12ENC; //开始转
TA0CTL = TASSEL__ACLK | MC__UP | TACLR; // ACLK, up mode

}