Other Parts Discussed in Thread: MSP430F4250
用了MSP430F4250对信息区的地址0x1040地址写数据并读取,结果好像写不进去,单步调试或者直接运行,在WATCH中看到这个地址的值一直是0xff,不知道什么原因,哪位高手帮忙看看,谢谢。
晶振是4M。
void main(void)
{
WDTCTL = WDTPW + WDTHOLD;
FLL_CTL0 |= XTS_FLL; //设置振荡器为高频,4M
FLL_CTL0 |= XCAP0PF; //设置内部晶体匹配电容为0PF
SCFQCTL = SCFQ_64K; //设置MCLK=SMCLK=2*ACLK;
FCTL2=FWKEY+FSSEL1+FN3+FN1;//FLASH时钟设置,选在MCLK,11分频,大约364K
char value=26;
char value_m=0;
char *data_ptr;
data_ptr=(char *)0x1040;
if(*data_ptr==0xff)
write_SegC(value);
else
value_m = *data_ptr;
}
void write_SegC(char value)
{
char *Flash_ptr; // Flash pointer
Flash_ptr = (char *)0x1040; // Initialize Flash pointer
FCTL3 = FWKEY; // Clear Lock bit
FCTL1 = FWKEY + ERASE; // Set Erase bit
*Flash_ptr = 0; // Dummy write to erase Flash seg
FCTL1 = FWKEY + WRT; // Set WRT bit for write operation
*Flash_ptr++ = value; // Write value to flash
FCTL1 = FWKEY; // Clear WRT bit
FCTL3 = FWKEY + LOCK; // Set LOCK bit
}