This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在MSP430 BSL 通信中80h 的使用



80 h 仅用于同步还是必须跟每个bootstrap loader 命令一起发送?

  • 在每次传输中80h 用于同步。芯片返回90h 作为响应,然后发送一个数据帧。每一帧以一个80h 的字节开头,帧其它字节紧跟在80h 之后。BSL 数据帧的格式在“Features of the MSP430 Bootstrap Loader”(文献编号SLAA089)有定义。,可以在MSP430网站上下载。在应用笔记“`Application of Bootstrap Loader in MSP430 w/Flash -Hardware and Software Proposal”(文献编号SLAA096)中,有详细的代码测试证明此技术的正确性。在应用笔记中提到的软件和硬件已经经过测试并且可以工作。