普通学生,最近在做东西的时候对fram的读写的C语言程序很迷糊,请问应该学习些什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
普通学生,最近在做东西的时候对fram的读写的C语言程序很迷糊,请问应该学习些什么?
#if defined(__TI_COMPILER_VERSION__)
#pragma PERSISTENT(FRAM_write)
unsigned long FRAM_write[WRITE_SIZE] = {0};
#elif defined(__IAR_SYSTEMS_ICC__)
__persistent unsigned long FRAM_write[WRITE_SIZE] = {0};
#elif defined(__GNUC__)
unsigned long __attribute__((persistent)) FRAM_write[WRITE_SIZE] = {0}; //???????
#else
#error Compiler not supported!
#endif
请问例程代码这段宏定义中的__((persistent)) FRAM_write[WRITE_SIZE] = {0}; 有什么意义,不太理解,查阅数据手册说的很模糊
Here is example code which should show you how to use data in FRAM.
#include <msp430.h> #define WRITE_SIZE 128 void FRAMWrite(void); unsigned char count = 0; unsigned long data; #if defined(__TI_COMPILER_VERSION__) #pragma PERSISTENT(FRAM_write) unsigned long FRAM_write[WRITE_SIZE] = {0}; #elif defined(__IAR_SYSTEMS_ICC__) __persistent unsigned long FRAM_write[WRITE_SIZE] = {0}; #elif defined(__GNUC__) unsigned long __attribute__((persistent)) FRAM_write[WRITE_SIZE] = {0}; #else #error Compiler not supported! #endif int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop WDT // Configure GPIO P1OUT &= ~BIT0; // Clear P1.0 output latch for a defined power-on state P1DIR |= BIT0; // Set P1.0 to output direction // Disable the GPIO power-on default high-impedance mode to activate // previously configured port settings PM5CTL0 &= ~LOCKLPM5; // Initialize dummy data data = 0x00010001; while(1) { data += 0x00010001; FRAMWrite(); count++; if (count > 100) { P1OUT ^= 0x01; // Toggle LED to show 512K bytes count = 0; // ..have been written data = 0x00010001; } } } void FRAMWrite(void) { unsigned int i = 0; for (i = 0; i < WRITE_SIZE; i++) { FRAM_write[i] = data; } }
你看到前面的#if defined没? 一般编译器如CCS,运行你这段程序时只会执行这句#pragma PERSISTENT(FRAM_write) 在FRAM中生成地址的。同理unsigned long __attribute__((persistent)) FRAM_write[WRITE_SIZE] = {0}; 的作用同#pragma PERSISTENT(FRAM_write) 只是编译器不同罢了。