This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F149通过P6.0和P6.1进行双通道单次AD转换时,P6.0和P6.1悬空时P6.0ADC转换结果为0,P6.1转换输出结果不为0 ,求指导错误,希望P6.1输出为0



/********************************************************************
开发板1602液晶显示ADC转换结果程序,显示输入到ADC的电压转换后的数字量和模拟电压大小
//MSP430单片机内部12位ADC,采用内部2.5V基准,单通道单次转换,中断模式,有精度误差
//通过杜邦线将需要转换的电压加入到ADC0,也就是P60,可以更改输入电压,最大显示量4095和2.5V

********************************************************************/

#include <msp430x14x.h>
#include "Config.h" //开发板配置头文件,主要配置IO端口信息
#include "1602.c"

static uchar Flag=0; //标志变量
uint TEMP0=0; //ADC值暂存变量 ,通道0
uint TEMP1=0; //ADC值暂存变量,通道1
uint temp,A1,A2,A3,A4,A5,A6,A7; //定义的变量,显示数据处理

//***********************************************************************
// 显示采集到的ADC数值,已修改
//***********************************************************************
void LCD_DisplayADC1()
{
LCD_write_char(0x00,0,0x30+A1); //在第一行显示数字量
LCD_write_char(0x01,0,0x30+A2);
LCD_write_char(0x02,0,0x30+A3);
LCD_write_char(0x03,0,0X30+A4);
}

void LCD_DisplayVoltage1() //在第二行显示模拟电压,0、1用来区别行
{
LCD_write_char(0x00,1,0x30+A5);
LCD_write_char(0x01,1,'.');
LCD_write_char(0x02,1,0x30+A6);
LCD_write_char(0x03,1,0X30+A7);
LCD_write_char(0x04,1,'V');
}
void LCD_DisplayADC2()
{
LCD_write_char(0x0a,0,0x30+A1); //在第一行显示数字量
LCD_write_char(0x0b,0,0x30+A2);
LCD_write_char(0x0c,0,0x30+A3);
LCD_write_char(0x0d,0,0X30+A4);
}

void LCD_DisplayVoltage2() //在第二行显示模拟电压,0、1用来区别行
{
LCD_write_char(0x0a,1,0x30+A5);
LCD_write_char(0x0b,1,'.');
LCD_write_char(0x0c,1,0x30+A6);
LCD_write_char(0x0d,1,0X30+A7);
LCD_write_char(0x0e,1,'V');
}
//*************************************************************************
// 数字量显示处理函数
//*************************************************************************
void Data_do(uint temp_d)
{
uint temp_1,temp_2;
A1=temp_d/1000; //分出千,百,十,和个位
temp_1=temp_d%1000;
A2=temp_1/100;
temp_2=temp_1%100;
A3=temp_2/10;
A4=temp_2%10;
}

//*************************************************************************
// 电压数据显示处理函数
//*************************************************************************
void Voltage_do(uint temp_d)
{
uint temp_1,temp_2;
ulong temp_3;

temp_3=(ulong)(temp_d)*250; //转换公式,ADC数字量转换为电压大小,注意数据类型
temp_d=temp_3/4095; //12位精度,除以4095

A5=temp_d/100; //分出百,十,和个位
temp_1=temp_d%100;
A6=temp_1/10;
temp_2=temp_1%10;
A7=temp_2;
}

//*************************************************************************
// ADC初始化程序,用于配置ADC相关寄存器 已修改
//*************************************************************************
void ADC_Init()
{
P6SEL|=0x02; //使能ADC通道
// ADC12CTL0= ADC12ON + SHT0_2 + REF2_5V + REFON+MSC; //打开内核,内部参考电压发生器打开,内部参考电压值为2.5V,多次采样控制(MSC),采样时间(SHT0_2)
ADC12CTL0= ADC12ON + SHT0_1 +MSC;
ADC12CTL1= SHP+CONSEQ_1; //采样信号源自采样定时器,序列通道单次转换
//ADC12MCTL0= SREF0; //参考电压源选择位0VR+=AVcc,VR-=AVss及通道选择,这里选择通道0
//ADC12MCTL1= SREF0 ; //参考电压源选择位为0,选择通道1
ADC12MCTL0= INCH_0; //参考电压源选择位0VR+=AVcc,VR-=AVss及通道选择,这里选择通道0
ADC12MCTL1= INCH_1+EOS; //参考电压源选择位为0,选择通道1
ADC12IE|= 0x02; //中断允许

ADC12CTL0|= ENC; //使能转换器



}

//*************************************************************************
// ADC中断服务程序 已改
//*************************************************************************
#pragma vector=ADC_VECTOR
__interrupt void ADC12ISR(void)
{
uchar j;
while((ADC12CTL1&0x01)==1); //检验ADC12BUSY位,如果ADC忙,则等待,否则读取ADC转换数值
Flag = 1 ;
TEMP0 = ADC12MEM0; //读取通道0,ADC转换值,存入变量TEMP0
TEMP1 = ADC12MEM1; //读取通道1,ADC转换值,存入变量TEMP1
Data_do(TEMP0); //处理ADC值,用于显示,数字量.通道0
Voltage_do(TEMP0); //处理ADC值,用于显示,模拟电压值,通道0
for(j=0;j<15;j++)
{
LCD_DisplayADC1(); //显示ADC的数据,ADC数字量
LCD_DisplayVoltage1(); //显示ADC的电压值
}
Data_do(TEMP1); //处理ADC值,用于显示,数字量.通道1
Voltage_do(TEMP1); //处理ADC值,用于显示,模拟电压值,通道1

for(j=0;j<15;j++)
{
LCD_DisplayADC2(); //显示ADC的数据,ADC数字量
LCD_DisplayVoltage2(); //显示ADC的电压值
}
}

//***********************************************************************
// 主程序
//***********************************************************************
void main(void)
{
WDT_Init(); //看门狗初始化
Clock_Init(); //时钟初始化
Port_Init(); //端口初始化,用于控制IO口输入或输出
ADC_Init(); //初始化ADC配置
delay_ms(100); //延时100ms
LCD_init(); //液晶参数初始化设置
LCD_clear(); //清屏
LCD_Desk();
_EINT(); //使能中断
Flag=1; //标志位先置1

while(1)
{
while(Flag==1)
{
ADC12CTL0 |= ADC12SC; //开启转换
ADC12CTL0 &= ~ADC12SC; //清零
Flag=0; //清零标志位
}
}
}