This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

G2332 AD采样问题

Dear  All

我们在使用MSP430G2332IPW20R进行AD采样的时候,不同产地的430MCU的AD精度不一样。我们检测4.00V的电压,采用电阻分压的方式进行采样,可接受的误差为+- 0.10V,只要检测到的电压在该范围内,会有一个反馈信号。但是产地是马来西亚的430MCU的精度比非马来西亚产的精度低0.08,意思是在检测3.90~4.10V电压时,马来西亚的产地的430MCU需要在3.82V时才能检测到最低的电压,但是其他产地的MCU只需在3.90V时,就能检测到最低的电压。这个有解决的办法吗?