This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EKG_1298模块的开发环境?

Other Parts Discussed in Thread: MSP430F5342, ADS1298, ADS1298R

大家好,

     我们拥有EKG1298模块的材料, 但如何生成EKG1298的可执行image, 用于下载执行?

     例如: 编译错误如下:

       

”
-i"D:/CCS_6.0/ccsv6/ccs_base/msp430/lib/5xx_6xx_FRxx" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="MSP430-Timer2_linkInfo.xml" --rom_model -o "MSP430-Timer2.out"  "./MSP430_ADS1298.obj" "../lnk_msp430f5342.cmd" -l"libc.a" -l"libmath.a" 
<Linking>
 undefined  first referenced    
  symbol        in file         
 ---------  ----------------    
 DAC12_1CTL ./MSP430_ADS1298.obj
 DAC12_1DAT ./MSP430_ADS1298.obj
 FLL_CTL0   ./MSP430_ADS1298.obj
>> Compilation failure
 OA0CTL0    ./MSP430_ADS1298.obj
 OA0CTL1    ./MSP430_ADS1298.obj
 OA1CTL0    ./MSP430_ADS1298.obj
 OA1CTL1    ./MSP430_ADS1298.obj
 SCFQCTL    ./MSP430_ADS1298.obj
 TACCR0     ./MSP430_ADS1298.obj
 TACCR1     ./MSP430_ADS1298.obj
 TACCTL1    ./MSP430_ADS1298.obj
 TACTL      ./MSP430_ADS1298.obj
谢谢!
  • 我们将这些变量的定义引出:
    #ifndef SFR_8BIT
    /* External references resolved by a device-specific linker command file */
    #define SFR_8BIT(address) extern volatile unsigned char address
    #define SFR_16BIT(address) extern volatile unsigned int address
    //#define SFR_20BIT(address) extern volatile unsigned int address
    typedef void (* __SFR_FARPTR)();
    #define SFR_20BIT(address) extern __SFR_FARPTR address
    #define SFR_32BIT(address) extern volatile unsigned long address

    #endif

    #if 1
    SFR_8BIT(OA0CTL0); /* OA0 Control register 0 */
    SFR_8BIT(OA0CTL1); /* OA0 Control register 1 */
    SFR_8BIT(OA1CTL0); /* OA1 Control register 0 */
    SFR_8BIT(OA1CTL1); /* OA1 Control register 1 */

    SFR_16BIT(DAC12_1CTL); /* DAC12_1 Control */
    SFR_16BIT(DAC12_1DAT); /* DAC12_1 Data */

    SFR_16BIT(ADC12CTL0); /* ADC12 Control 0 */
    SFR_16BIT(ADC12CTL1); /* ADC12 Control 1 */
    SFR_16BIT(ADC12IFG); /* ADC12 Interrupt Flag */
    SFR_16BIT(ADC12IE); /* ADC12 Interrupt Enable */
    SFR_16BIT(ADC12IV); /* ADC12 Interrupt Vector Word */

    SFR_16BIT(TACTL); /* Timer A Control */

    SFR_16BIT(TACCR0); /* Timer A Capture/Compare 0 */
    SFR_16BIT(TACCR1); /* Timer A Capture/Compare 1 */

    SFR_8BIT(BTCTL); /* Basic Timer Control */
    #define XCAP18PF (0x30) /* XIN Cap = XOUT Cap = 18pf */

    #define LFOF (0x02) /* Low Frequency Oscillator Fault Flag */

    SFR_8BIT(FLL_CTL0); /* FLL+ Control 0 */


    SFR_8BIT(SCFQCTL); /* System Clock Frequency Control */

    #define CONSEQ_2 (2*2u) /* ADC12 Conversion Sequence Select: 2 */


    #define DAC12AMP_2 (2*0x0020u) /* DAC12 amplifier 2: low, low */
    #define DAC12CALON (0x0200) /* DAC12 calibration */
    #define DAC12ENC (0x0002) /* DAC12 enable conversion */
    #define DAC12IR (0x0100) /* DAC12 input reference and output range */

    #define ENC (0x002) /* ADC12 Enable Conversion */

    #define OAADC1 (0x02) /* OAx output to ADC12 input channel select 1 */

    #define OAP_0 (0x00) /* OAx Non-inverting input select 00 */
    #define OAP_1 (0x10) /* OAx Non-inverting input select 01 */
    #define OAP_2 (0x20) /* OAx Non-inverting input select 10 */
    #define OAP_3 (0x30) /* OAx Non-inverting input select 11 */

    #define OAPM_1 (0x04) /* OAx Power mode select: slow */

    #define OARRIP (0x01) /* OAx Rail-to-Rail Input off */

    #define REF2_5V (0x040) /* ADC12 Ref 0:1.5V / 1:2.5V */

    #define SHP (0x0200) /* ADC12 Sample/Hold Pulse Mode */

    #define SHS_1 (1*0x400u) /* ADC12 Sample/Hold Source: 1 */

    #define INCH_1 (1) /* ADC12 Input Channel 1 */


    #define SHT0_4 (4*0x100u) /* ADC12 Sample Hold 0 Select Bit: 4 */

    #define SREF_1 (1*0x10u) /* ADC12 Select Reference 1 */

    SFR_16BIT(TACCTL1); /* Timer A Capture/Compare Control 1 */

    #endif

    但错误结果如上所示!
  • 能否提供下完整的模块名字,搜索EKG1298找不到这个模块
  • 您现在用的是 ADS1298R ECGFE?
  • 是,

    编译该如何处理?
  • 请问您现在是编译的是哪个code?

    您可以试一下 e2e.ti.com/.../60104 给出的程序