Other Parts Discussed in Thread: MSP430I2041
您好!
最近在调msp430i2041外设SD24检测电压,遇到了几个问题,希望您能帮忙指导下。
1、数据手册说内部参考电压是1.2V,但是我需要检测的电压值最大2V多,所以只能采用外部参考电压,请问外部参考电压该怎么接?现在原理图接法是A3.0+接检测端,A3.0-接GND,VREF串个0.1uf接GDN。
2、如下是个简单的测试程序:
unsigned long int results; // SD24 Conversion Results
void main(void){
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
//SD24CTL = SD24REFS; // Internal ref
SD24CCTL3 |= SD24SNGL |SD24DF; // Single sample, 2's complement
//SD24INCTL3 |= SD24INCH_3;
__delay_cycles(3200); // Delay ~200us for 1.2V ref to settle
while(1)
{
SD24CCTL3 |= SD24SC; // Set bit to start conversion
while(!(SD24CCTL3 & SD24IFG)); // Poll IFG until conversion completes
results = SD24MEM3; // Save SD24 conversion results
__no_operation(); // SET BREAKPOINT HERE
}
}
最大只能检测到0.6V,超过0.6V的电压,AD值满量程输出为32768,请问怎么扩大检测范围?
3、该AD采样为24位,怎么得到一个24位值?
谢谢您!