This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在MSP430 C语言编程中为什么有的寄存器可以使用 |= 来置位,有的寄存器却不能这样使用?

Other Parts Discussed in Thread: MSP430FR2422

最近在使用MSP430FR2422 的ADC, 参考了TI提供的例子程序。发现如下代码:

“ 

// Configure ADC10
ADCCTL0 &= ~ADCENC; // Disable ADC
ADCCTL0 = ADCSHT_2 | ADCON; // ADCON, S&H=16 ADC clks
ADCCTL1 = ADCSHP; // ADCCLK = MODOSC; sampling timer
ADCCTL2 = ADCRES; // 10-bit conversion results
ADCIE = ADCIE0; // Enable ADC conv complete interrupt
ADCMCTL0 = ADCINCH_13 | ADCSREF_0; // A13 ADC input select = 1.5V Ref
// Vref = DVCC
// Configure reference module located in the PMM
PMMCTL0_H = PMMPW_H; // Unlock the PMM registers
PMMCTL2 |= INTREFEN; // Enable internal reference
while(!(PMMCTL2 & REFGENRDY)); // Poll till internal reference settles

”

发现有时候寄存器使用了标准的|= ,而有时候却直接用了=。 开始以为是例子程序写的时候忘记加| ,因此就都给补上了|, 但程序运行中发现ADC没有工作起来,采样值为0x000. 研究了很长时间发现,将程序复原为上述例子程序中的那样则ADC能正常工作。很是费解。请帮忙解释一下。非常感谢。

Brian