This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【问题求解】有关CCS8的使用问题

我是一名学生,使用的是MSP430F5529LP,软件是CCS8,以前一直使用的是寄存器版本的开发,现在想用使用库函数开发,我在网上找了很多的回答,都不是很详细,我尝试了很多次,还是没有能完全解决我的问题,第一,在MSPWARE下面有很多个driverlib文件夹,不确定添加的时候添加那个文件夹,第二,我任意添加driverlib进工程去之后,在include option里面添加了路径,结果在c文件里面头文件包含的时候要添加你想要添加的.h文件的完整路径,C:\ti\......\adc12_a.这样的,第三,我在MSP430F5xx_6xx_DriverLib_Users_Guide-2_91_07_07里面看到建立库函数工程的方法,但是在选择工程类型的时候没有包含驱动库的那个类型,第四,再给已存在的工程里面包含驱动库的时候,右键点击工程选择source,apply project template,结构里面是空的,没有 add copty of driverlib to project和 point to installed dirverlib,这是什么原因呢?哪位能帮我介绍下建立库函数版本的工程的步骤吗?