This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VLOCLK有没有启动时间?



VLOCLK有没有启动时间?

例如如果要从LPM4进入更高功耗的模式,要不要考虑启动时间?

如果在LPM4模式中中断,是不是在中断中,辅助时钟也会在中断开始的时候自动启动?

不管在何种低功耗模式,关于中断时SR压栈后 CPUOFF, SCG1, and OSCOFF 复位,那么在中断中时钟的运行之类的情况是否有可能值得关注的地方?

  • 任何CLK启动都是需要时间的,这个启动时间实际上就是从各种低功耗模式切换到更高一级的模式的切换时间中了.所以从LPM4模式进入更高的低功耗模式时,程序员不需要关心CLK的启动时间。

    从LPM4进入中断后,被保存的SR寄存器会从堆栈POP出来,换句话说系统会恢复到你进入LPM4模式之前的状态。所以你关心的问题就变成了一个,哪就是你进入LPM4低功耗模式之前,要考虑哪些中断会唤醒,在这些中断中哪些CLK会被需要用到。

  • 从LPM4进入中断后,被保存的SR寄存器会从堆栈POP出来,换句话说系统会恢复到你进入LPM4模式之前的状态。

    请问进入中断还是退出中断?

    5.  The interrupt request flag resets automatically on single-source flags. Multiple source flags remain set

    for servicing by software.

    任何CLK启动都是需要时间的,这个启动时间实际上就是从各种低功耗模式切换到更高一级的模式的切换时间中了.

    请问如果是使用外部晶体的 LFXT1CLK的ACLK呢?