This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MSP430x1xx(不包括 MSP430P112) 和MSP430x4xx 在 8MHz 时VCC 的推荐值为多少?
你好,当我们说工作电压时一般是指一个伏值范围,3.6V是个推荐值,那么8M频率时能正常工作的电压范围是什么呢?比如说3.6V以上都可以呢?还是3.3V至3.6V呢?
主频需要最低工作电压支持,范围是(MIN=主频所需的最低工作电压,MAX=MCU的最高工作电压)
MSP430x1xx的工作电压范围是(1.8v,3,6V),而主频在8Mhz时,最低工作电压是3.6V。
所以对MSP430X1xx来讲,只能工作在3.6V的电压点上。
你好,
我用MSP430, 电压低到2.0仍然正常工作。
另外“主频在8Mhz时,最低工作电压是3.6V”,那最高工作电压呢?