This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Msp432p401能用在程序中随时访问TA定时器的TAR计数值吗?



Msp432p401能用在程序中随时访问TA定时器的TAR计数值吗?访问丅AR的值及时准确不?

  • 您可以尝试使用 Timer_A_getCounterValue

    uint16_t Timer_A_getCounterValue ( uint32_t  timer )

    Returns the current value of the specified timer. Note that according to the Timer A user guide, reading the value of the counter is unreliable if the system clock is asynchronous from the timer clock. The API addresses this concern by reading the timer count register twice and then determining the integrity of the value. If the two values are within 10 timer counts of each other, the value is deemed safe and returned. If not, the process is repeated until a reliable timer value is determined.

    Parameters
    timer is the instance of the Timer_A module. Valid parameters vary from part to part, but can include:
    • TIMER_A0_BASE
    • TIMER_A1_BASE
    • TIMER_A2_BASE
    • TIMER_A3_BASE
    Returns
    The value of the specified timer

    References TIMER_A_CMSIS, and TIMER_A_THRESHOLD.

    另外建议您阅读以下 TRM 的 19.2.1 16-Bit Timer Counter

    The 16-bit timer/counter register, TAxR, increments or decrements (depending on mode of operation) with each rising edge of the clock signal. TAxR can be read or written with software. Additionally, the timer can generate an interrupt when it overflows.

    TAxR may be cleared by setting the TACLR bit. Setting TACLR also clears the clock divider and count direction for up/down mode.

    NOTE: Modifying Timer_A registers It is recommended to stop the timer before modifying its operation (with exception of the interrupt enable, interrupt flag, and TACLR) to avoid errant operating conditions. When the timer clock is asynchronous to the CPU clock, any read from TAxR should occur while the timer is not operating or the results may be unpredictable. Alternatively, the timer may be read multiple times while operating, and a majority vote taken in software to determine the correct reading. Any write to TAxR takes effect immediately.