This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lcd12864 在msp430f5529上无法显示



在网上找的源程序, 但在5529上不能实现,5529要怎么接12864的引脚 我想让5529接受ADC采集在12864上显示出来,下面的程序只是12864显示程序

#include "msp430.h"
#define CPU_F ((double)8000000)
#define delay_us(x) __delay_cycles((long)(CPU_F*(double)x/1000000.0))
#define delay_ms(x) __delay_cycles((long)(CPU_F*(double)x/1000.0))

#define uchar unsigned char
#define uint unsigned int
#define ulong unsigned long

/*12864应用指令*/
#define CLEAR_SCREEN 0x01 //清屏指令:清屏且AC值为00H
#define AC_INIT 0x02 //将AC设置为00H。且游标移到原点位置
#define CURSE_ADD 0x06 //设定游标移到方向及图像整体移动方向(默认游标右移,图像整体不动)
#define FUN_MODE 0x30 //工作模式:8位基本指令集
#define DISPLAY_ON 0x0c //显示开,显示游标,且游标位置反白
#define DISPLAY_OFF 0x08 //显示关
#define CURSE_DIR 0x14 //游标向右移动:AC=AC+1
#define SET_CG_AC 0x40 //设置AC,范围为:00H~3FH
#define SET_DD_AC 0x80

#define RS_CLR P2OUT &= ~BIT7 //RS置低
#define RS_SET P2OUT |= BIT7 //RS置高

#define RW_CLR P2OUT &= ~BIT6 //RW置低
#define RW_SET P2OUT |= BIT6 //RW置高

#define EN_CLR P2OUT &= ~BIT5 //E置低
#define EN_SET P2OUT |= BIT5 //E置高

#define DataPort P3OUT //P3口为数据口


//*************************************************************************
// 系统时钟初始化
//*************************************************************************
void Clock_Init()
{
UCSCTL1 = DCORSEL_2; // 设置DCO范围
UCSCTL3 |= SELREF_2; // 选择FLL参考源自REFO
UCSCTL4 = SELM_3 + SELA_2 + SELS_4; // 配置 MCLK = DCOC,SMCLK =DCODIV,ACLK=REFO
while (SFRIFG1 & OFIFG) // 清除 OFIFG,and XT1OFFG ,DCOFFG
{
UCSCTL7 &= ~( XT1LFOFFG + DCOFFG);
SFRIFG1 &= ~OFIFG;
}
}

//*************************************************************************
// MSP430内部看门狗初始化
//*************************************************************************
void WDT_Init()
{
WDTCTL = WDTPW + WDTHOLD; //关闭看门狗
}

//*************************************************************************
// 初始化IO口子程序
//*************************************************************************
void Port_init()
{

P3SEL = 0x00;
P3DIR = 0xFF;
P2SEL = 0x00;
P2DIR|= BIT5 + BIT6 +BIT7;
}

//***********************************************************************
// 显示屏命令写入函数
//***********************************************************************


void LCD_write_com(unsigned char com)
{
RS_CLR;
RW_CLR;
EN_SET;
DataPort = com;
delay_ms(5);
EN_CLR;
}
//***********************************************************************
// 显示屏数据写入函数
//***********************************************************************

void LCD_write_data(unsigned char data)
{
RS_SET;
RW_CLR;
EN_SET;
DataPort = data;
delay_ms(5);
EN_CLR;
}
//***********************************************************************
// 显示屏清空显示
//***********************************************************************

void LCD_clear(void)
{
LCD_write_com(0x01);
delay_ms(5);
}

//***********************************************************************
//函数名称:DisplayCgrom(uchar hz)显示CGROM里的汉字
//***********************************************************************
void DisplayCgrom(uchar addr,uchar *hz)
{
LCD_write_com(addr);
delay_ms(5);
while(*hz != '\0')
{
LCD_write_data(*hz);
hz++;
delay_ms(5);
}

}
//****************************************************************
//函数名称:Display()显示测试结果
//****************************************************************
void Display(void)
{
DisplayCgrom(0x80,"测试程序");
DisplayCgrom(0x88,"helloworld");
DisplayCgrom(0x90,"helloworld");
DisplayCgrom(0x98,"12344667");

}

//***********************************************************************
// 显示屏初始化函数
//***********************************************************************

void LCD_init(void)
{
LCD_write_com(FUN_MODE); //显示模式设置
delay_ms(5);
LCD_write_com(FUN_MODE); //显示模式设置
delay_ms(5);
LCD_write_com(DISPLAY_ON); //显示开
delay_ms(5);
LCD_write_com(CLEAR_SCREEN); //清屏
delay_ms(5);
}
//***********************************************************************
// 主程序
//***********************************************************************
void main(void)
{
WDT_Init(); //看门狗设置
Clock_Init(); //系统时钟设置
Port_init(); //系统初始化,设置IO口属性
delay_ms(100); //延时100ms
LCD_init(); //液晶参数初始化设置
LCD_clear(); //清屏
while(1)
{
Display(); //显示汉字
}
}