Other Parts Discussed in Thread: MSP430G2553
我希望在按键中断中,拉高P1.7,同时定时一分钟,一分钟后拉低P1.7,该怎么写呢?
我目前的代码如下:
#include"msp430g2553.h"
void delay(int time)
{
static int i,j;
for(i=0;i<time;i++)
{ for(j=0;j<128;j++);}
}
void InitIOInterrupt()
{
P1DIR &= ~BIT3;//设置P1.3为输入
P1REN |= BIT3;//启用P1.3电阻
P1OUT |= BIT3;//设置上拉电阻
P1IES |= BIT3;//P1.3中断边缘选择
P1IE |= BIT3;//P1.3中断使能
P1IFG = 0x00;//清除中断标识
}
void InitLed()
{
P1DIR |= BIT7;//设置BIT7为输出
P1OUT &= 0x00; //设置BIT7低电平
}
#pragma vector=PORT1_VECTOR //按键中断
__interrupt void PORT1_ISR(void)
{
static int k;
delay(50);
P1OUT = 0x80;//P1.7置高
P1IFG = 0;//清除中断标识
}
void main()
{
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
//DCOCTL = CALDCO_1MHZ;
//BCSCTL1 = CALBC1_1MHZ;
InitLed(); //初始化输出端口
InitIOInterrupt(); //初始化IO中断
_EINT(); //开总中断
while(1);
}