Other Parts Discussed in Thread: MSP430F5529
hi,ti的工程师你们好,我遇到了一个问题,请帮忙看看。
使用的硬件;msp430f5529 launchpad
软件;tirtos tirtos_msp43x_2_20_00_06
我的目标是实现可以同时使用两个spi。
问题:tirtos在使用spi的时候需要用到dma的中断,但是因为用了两个spi,在调用SPI_serviceISR函数时有问题。所以怎样设置.cfg里面的中断,才能让SPI_serviceISR()正确的工作?????????
部分代码如下:
Void MSP_EXP430F5529LP_isrDMA(UArg arg)
{
/* Call the SPI DMA function, passing the SPI handle used for WiFi */
SPI_serviceISR((SPI_Handle) &(SPI_config[1])); //这里的入参应该是根据调用的是SPI_config[0]或者SPI_config[1],但是不知道怎么传递过来
//我尝试在这边加入全局变量来判断,但是程序在运行第二次SPI_transfer的时候就卡住了
}
///////////.cfg文件里增加
var hwiParams = new halHwi.Params();
hwiParams.arg = 0; //////////////如何修改这里为一个变量?????????????????????????????????????????
halHwi.create(50, "&MSP_EXP430F5529LP_isrDMA", hwiParams);
/////////////////////////
/*
* =============================== SPI ===============================
*/
/* Place into subsections to allow the TI linker to remove items properly */
#if defined(__TI_COMPILER_VERSION__)
#pragma DATA_SECTION(SPI_config, ".const:SPI_config")
#pragma DATA_SECTION(spiUSCIBDMAHWAttrs, ".const:spiUSCIBDMAHWAttrs")
#endif
#include <ti/drivers/SPI.h>
#include <ti/drivers/spi/SPIUSCIADMA.h>
#include <ti/drivers/spi/SPIUSCIBDMA.h>
SPIUSCIADMA_Object spiUSCIADMAObjects[MSP_EXP430F5529LP_SPICOUNT]; ///MSP_EXP430F5529LP_SPICOUNT =1
SPIUSCIBDMA_Object spiUSCIBDMAObjects[MSP_EXP430F5529LP_SPICOUNT];
uint8_t spiUSCIADMAscratchBuf[MSP_EXP430F5529LP_SPICOUNT];
uint8_t spiUSCIBDMAscratchBuf[MSP_EXP430F5529LP_SPICOUNT];
const SPIUSCIBDMA_HWAttrs spiUSCIBDMAHWAttrs[MSP_EXP430F5529LP_SPICOUNT] = {
{
.baseAddr = USCI_B0_BASE,
.clockSource = USCI_B_SPI_CLOCKSOURCE_SMCLK,
.bitOrder = USCI_B_SPI_MSB_FIRST,
.scratchBufPtr = &spiUSCIBDMAscratchBuf[0],
.defaultTxBufValue = 0,
/* DMA */
.dmaBaseAddr = DMA_BASE,
/* Rx Channel */
.rxDMAChannelIndex = DMA_CHANNEL_2,
.rxDMASourceTrigger = DMA_TRIGGERSOURCE_18,
/* Tx Channel */
.txDMAChannelIndex = DMA_CHANNEL_0,
.txDMASourceTrigger = DMA_TRIGGERSOURCE_19
}
};
const SPIUSCIADMA_HWAttrs spiUSCIADMAHWAttrs[MSP_EXP430F5529LP_SPICOUNT] = {
{
.baseAddr = USCI_A0_BASE,
.clockSource = USCI_A_SPI_CLOCKSOURCE_SMCLK,
.bitOrder = USCI_A_SPI_MSB_FIRST,
.scratchBufPtr = &spiUSCIADMAscratchBuf[0],
.defaultTxBufValue = 0,
/* DMA */
.dmaBaseAddr = DMA_BASE,
/* Rx Channel */
.rxDMAChannelIndex = DMA_CHANNEL_2,
.rxDMASourceTrigger = DMA_TRIGGERSOURCE_16,
/* Tx Channel */
.txDMAChannelIndex = DMA_CHANNEL_0,
.txDMASourceTrigger = DMA_TRIGGERSOURCE_17
}
};
const SPI_Config SPI_config[] = {
{
.fxnTablePtr = &SPIUSCIBDMA_fxnTable,
.object = &spiUSCIBDMAObjects[0],
.hwAttrs = &spiUSCIBDMAHWAttrs[0]
},
{
.fxnTablePtr = &SPIUSCIADMA_fxnTable,
.object = &spiUSCIADMAObjects[0],
.hwAttrs = &spiUSCIADMAHWAttrs[0]
},
// {NULL, NULL, NULL},
};
/*
* ======== MSP_EXP430F5529LP_initSPI ========
*/
void MSP_EXP430F5529LP_initSPI(void)
{
/*
* NOTE: TI-RTOS examples configure USCIB0 as either SPI or I2C. Thus,
* a conflict occurs when the I2C & SPI drivers are used simultaneously in
* an application. Modify the pin mux settings in this file and resolve the
* conflict before running your the application.
*/
/* SPI CLK */
GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P3, GPIO_PIN2);
/* MOSI/SIMO */
GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P3, GPIO_PIN0);
/* MISO/SOMI */
GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P3, GPIO_PIN1);
/* SPI CLK */
GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P2, GPIO_PIN7);
/* MOSI/SIMO */
GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P3, GPIO_PIN3);
/* MISO/SOMI */
GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P3, GPIO_PIN4);
SPI_init();
}
我已经确认了的事情:
1,单独使用其中一个配置是没有问题的。
2,两个同时用到 时候问题出在没有正确的进入SPI_serviceISR()函数。这个函数需要传入正确的入参,但是我没有找到正确的方法。