This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6972单片机内部DCO可以关闭吗?

Other Parts Discussed in Thread: MSP430FR6972

MSP430FR6972单片机内部DCO可以关闭吗?最近遇见一个问题:当外部32K晶振停振或者出现异常的时候,单片机会自动切换到内部39K,功耗很大约140μA左右,此时硬串口也无法通讯。

  • 当外部晶振出现问题时会自动切换到内部DCO.当进入低功耗3模式时,DCO停止。
    您现在是想实现什么功能呢?
  • 我们用6972单片机做了一个款产品,使用了一款新的晶振,现在已经确定程序容易死到初始化时钟子函数中,因为里面有做判断晶振失效标志的死循环do{…}while(…),用示波器测试32k晶振起振,示波器探头一离开晶振,单片机自动又切换到内部晶振,现在不能确定晶振到底是振了没有?程序有定时1小时初始化晶振,依然不会切换到外部晶振。
  • 无源晶振经常出现这种问题,可能是无源晶振的电路以及PCB布局有问题导致的。一旦失效系统自动切换到内置RC振荡器。
  • 你这个切换时钟的现象可以在用户手册的3.2.8 CS Module Fail-Safe Operation看到。建议仔细阅读以下。

    另外,关于外部晶振的问题,你可以参考这个技术文档:www.ti.com/.../slaa322d.pdf

    还有,内部有VLO(低频)和MODCLK(高频)两个片上晶振,功耗水平非常不错的。你可以考虑以下。

    www.ti.com/.../slau367o.pdf