This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430f149中ad采集的问题

为什么我进行在线调试的时候,在Register栏中查看MEM0,MEM1,MEM2,MEM3都是0000,这说明AD没有采样成功而且采样的值也没有写入MEMX寄存器吗?我该怎么解决,求告知,谢谢!!下面是我的程序:

#include<msp430.h>
#define Num_of_Results 32
#define ulong unsigned long
#define uint unsigned int
#define uchar unsigned char
ulong caltmp[4];
static uint results[Num_of_Results]; //保存ADC转换结果的数组
uint i;
/********************************************
函数名称:Init_ADC
功 能:初始化ADC
参 数:无
返回值 :无
********************************************/
void Init_ADC(void)
{
P6SEL |= 0x0f; // 使能ADC通道
ADC12CTL0 = ADC12ON+SHT0_15+MSC; // 打开ADC,设置采样时间
ADC12CTL1 = SHP+CONSEQ_3+CSTARTADD2; // 使用采样定时器,脉冲模式+单通道多次转换
ADC12MCTL0=INCH_0;
ADC12MCTL1=INCH_1;
ADC12MCTL2=INCH_2;
ADC12MCTL3=INCH_3+EOS; //以EOS结束此次转换
ADC12IE = 0x0f; // 使能ADC中断
//ADC12IV=ADC12IV_ADC12IFG3;
ADC12CTL0 |= ENC; // 使能转换
ADC12CTL0 |= ADC12SC; // 开始转换
// _BIS_SR(LPM0_bits + GIE);
for(i=0;i<50;i++)
_NOP();
_EINT();
//_BIS_SR(LPM0_bits + GIE);
}

函数名称:ADC12ISR
功 能:ADC中断服务函数,在这里用多次平均的
计算P6.0口的模拟电压数值
参 数:无
返回值 :无
********************************************/
#pragma vector=ADC_VECTOR
__interrupt void ADC12ISR(void)
{
//while((ADC12CTL1&0X01)==1);
caltmp[0]=ADC12MEM0;
caltmp[1]=ADC12MEM1;
caltmp[2]=ADC12MEM2;
caltmp[3]=ADC12MEM3;

}

/******************************************************************************************************************/

主程序

#include <msp430.h>
#include"AD_BAT.c"


#define uint unsigned int
#define uchar unsigned char
int main( void )
{
// Stop watchdog timer to prevent time out reset
WDTCTL = WDTPW + WDTHOLD;
BCSCTL1 &= ~XT2OFF; //打开XT2高频晶体振荡器
uchar i,j;
do
{
IFG1 &= ~OFIFG; //清除晶振失败标志
for (i = 0xFF; i > 0; i--); //等待8MHz晶体起振
}
while ((IFG1 & OFIFG)); //晶振失效标志仍然存在?(判断晶振是否起振)
BCSCTL2 |= SELM_2 + SELS; //MCLK和SMCLK选择高频晶振
TACTL |= TASSEL_2 + ID_3; //计数时钟选择SMLK=8MHz,1/8分频后为1MHz
//_EINT();
Init_ADC();
for(j=0;j<100;j++)
_NOP();

return 0;
}

  • /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2012, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     * 
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //  MSP-FET430P140 Demo - ADC12, Sequence of Conversions (non-repeated)
    //
    //  Description: This example shows how to perform A/D conversions on a sequence
    //  of channels. A single sequence of conversions is performed - one conversion
    //  each on channels A0, A1, A2, and A3. Each conversion uses AVcc and AVss for
    //  the references. The conversion results are stored in ADC12MEM0, ADC12MEM1,
    //  ADC12MEM2, and ADC12MEM3 respectively and are moved to 'results[]' upon
    //  completion of the sequence. Test by applying voltages to pins A0, A1, A2,
    //  and A3, then setting and running to a break point at the "_BIC..."
    //  instruction in the ISR. To view the conversion results, open a watch window
    //  in debugger and view 'results' or view ADC12MEM0, ADC12MEM1, ADC12MEM2, and
    //  ADC12MEM3 in an ADC12 SFR window.
    //  This can run even in LPM4 mode as ADC has its own clock
    //  Note that a sequence has no restrictions on which channels are converted.
    //  For example, a valid sequence could be A0, A3, A2, A4, A2, A1, A0, and A7.
    //  See the MSP430x1xx User's Guide for instructions on using the ADC12.
    //
    //
    //                MSP430F149
    //            -----------------
    //           |                 |
    //   Vin0 -->|P6.0/A0          |
    //   Vin1 -->|P6.1/A1          |
    //   Vin2 -->|P6.2/A2          |
    //   Vin3 -->|P6.3/A3          |
    //           |                 |
    //
    //
    //  M. Mitchell
    //  Texas Instruments Inc.
    //  Feb 2005
    //  Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.21A
    //******************************************************************************
    
    #include <msp430.h>
    
    static unsigned int results[4];             // Needs to be global in this example
                                                // Otherwise, the compiler removes it
                                                // because it is not used for anything.
    
    int main(void)
    {
      WDTCTL = WDTPW+WDTHOLD;                   // Stop watchdog timer
      P6SEL = 0x0F;                             // Enable A/D channel inputs
      ADC12CTL0 = ADC12ON+MSC+SHT0_2;           // Turn on ADC12, set sampling time
      ADC12CTL1 = SHP+CONSEQ_1;                 // Use sampling timer, single sequence
      ADC12MCTL0 = INCH_0;                      // ref+=AVcc, channel = A0
      ADC12MCTL1 = INCH_1;                      // ref+=AVcc, channel = A1
      ADC12MCTL2 = INCH_2;                      // ref+=AVcc, channel = A2
      ADC12MCTL3 = INCH_3+EOS;                  // ref+=AVcc, channel = A3, end seq.
      ADC12IE = 0x08;                           // Enable ADC12IFG.3
      ADC12CTL0 |= ENC;                         // Enable conversions
    
      while(1)
      {
      ADC12CTL0 |= ADC12SC;                     // Start conversion
      __bis_SR_register(LPM0_bits + GIE);       // Enter LPM0, Enable interrupts
      }
    }
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=ADC12_VECTOR
    __interrupt void ADC12ISR (void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(ADC12_VECTOR))) ADC12ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
      results[0] = ADC12MEM0;                   // Move results, IFG is cleared
      results[1] = ADC12MEM1;                   // Move results, IFG is cleared
      results[2] = ADC12MEM2;                   // Move results, IFG is cleared
      results[3] = ADC12MEM3;                   // Move results, IFG is cleared
      __bic_SR_register_on_exit(LPM0_bits);     // Clear LPM0, SET BREAKPOINT HERE
    }

    给你个参考,跟你的非常类似了,你看看你的是咋回事。你用了中断,但是你中断的名字好像定义的都不大对
  • 您好,请问为什么我编译这个程序时会有一个警告,就是results 定义了但未被使用
  • 您好,请问为什么我编译这个程序时会有一个警告,就是results 定义了但未被使用