各位工程师:
您好!我想问一下使用MSP430F5529 Launchpad时,可不可以将程序直接下载至仿真器部分MSP430F5528中,也就是这个5528系统我们可以用吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位工程师:
您好!我想问一下使用MSP430F5529 Launchpad时,可不可以将程序直接下载至仿真器部分MSP430F5528中,也就是这个5528系统我们可以用吗?
板子上有 eZ-FET lite Emulator,可以给其他的430器件来烧录程序
The eZ-FET lite is simple and low cost. Like the emulator on the G2 LaunchPad development kit (MSPEXP430G2), it provides a "backchannel" UART-over-USB connection with the host, which can be very useful during debugging. But unlike the G2 emulator, it:
• supports almost all MSP430 MCUs
• has a configurable backchannel UART baudrate
• is completely open source!
在MSP430F5529LP中MSP430F5528是作为eZ-FET lite Emulator的一部分,是用于烧录程序的。您现在是想如何用?能否请您详细说一下?