This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
按照MSP430F673x_672x的示范代码:MSP430F673X_USCIA0_UART_04.c
#include <msp430.h> int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop WDT // Setup P1.2 UCA0RXD, P1.3 UCA0TXD P1SEL |= BIT2 | BIT3; // Set P1.2, P1.3 to non-IO P1DIR |= BIT2 | BIT3; // Enable UCA0RXD, UCA0TXD // Setup LFXT1 UCSCTL6 &= ~(XT1OFF); // XT1 On UCSCTL6 |= XCAP_3; // Internal load cap // Loop until XT1 fault flag is cleared do { UCSCTL7 &= ~(XT2OFFG | XT1LFOFFG | DCOFFG); // Clear XT2,XT1,DCO fault flags SFRIFG1 &= ~OFIFG; // Clear fault flags } while (SFRIFG1 & OFIFG); // Test oscillator fault flag // Setup eUSCI_A0 UCA0CTLW0 |= UCSWRST; // **Put state machine in reset** UCA0CTLW0 |= UCSSEL_2; // SMCLK UCA0BRW_L = 6; // 1MHz 9600 (see User's Guide) UCA0BRW_H = 0; // 1MHz 9600 UCA0MCTLW = UCBRF_13 | UCOS16; // Modln UCBRSx=0, UCBRFx=0x13, // over sampling UCA0CTLW0 &= ~UCSWRST; // **Initialize USCI state machine** UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt __bis_SR_register(LPM0_bits | GIE); // Enter LPM0, interrupts enabled __no_operation(); // For debugger } // USCI_A0 interrupt service routine #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector=USCI_A0_VECTOR __interrupt void USCI_A0_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void) #else #error Compiler not supported! #endif { switch (__even_in_range(UCA0IV, 4)) { case USCI_NONE: break; // No interrupt case USCI_UART_UCRXIFG: // RXIFG while (!(UCA0IFG & UCTXIFG)) ; // USCI_A0 TX buffer ready? UCA0TXBUF = UCA0RXBUF; // TX -> RXed character break; case USCI_UART_UCTXIFG: break; // TXIFG case USCI_UART_UCSTTIFG: break; // TTIFG case USCI_UART_UCTXCPTIFG: break; // TXCPTIFG default: break; } }
我仅仅把串口1换成了串口2,然后就发现通讯不正常,最后把串口助手的波特率设为2400,就接收正确。
中断也能进去。发什么收什么。
我的代码:(我加了TA1定时中断,闪灯测试一秒钟闪两次)
//****************************************************************************** #include <msp430f6723.h> int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop WDT // Setup P2.2 UCA0RXD, P2.3 UCA0TXD P2SEL |= BIT2 | BIT3; // Set P2.2, P2.3 to non-IO, Peripheral function select : 1 P2DIR |= BIT3; // Enable UCA2RXD, UCA2TXD 0: input for RxD, 1: output for TxD P2DIR &= ~BIT2; P5DIR |= 0x01; // Set P5.0 to output direction // Setup LFXT1 UCSCTL6 &= ~(XT1OFF); // XT1 On UCSCTL6 |= XCAP_3; // Internal load cap // Loop until XT1 fault flag is cleared do { UCSCTL7 &= ~(XT2OFFG | XT1LFOFFG | DCOFFG); // Clear XT2,XT1,DCO fault flags SFRIFG1 &= ~OFIFG; // Clear fault flags } while (SFRIFG1 & OFIFG); // Test oscillator fault flag // Setup eUSCI_A2 UCA2CTLW0 |= UCSWRST; // **Put state machine in reset** // UCSYNC UCA2CTLW0 |= UCSSEL__SMCLK; // SMCLK UCA2BRW_L = 1; // 1MHz 9600 (see User's Guide) UCA2BRW_H = 0; // 1MHz 9600 UCA2MCTLW = UCBRF_11 | UCOS16 | 0x2500; // Modln UCBRSx=0, UCBRFx=0x13, // over sampling UCA2CTLW0 &= ~UCSWRST; // **Initialize USCI state machine** UCA2IE = UCRXIE; // Enable USCI_A2 RX interrupt // Setup TA1 TA1CCTL0 = CCIE; // CCR0 interrupt enabled TA1CCR0 = 65535; TA1CTL = TASSEL_2 | MC_2 | TACLR; // SMCLK, contmode, clear TAR //__bis_SR_register(GIE); __bis_SR_register(LPM0_bits | GIE); // Enter LPM0, interrupts enabled __no_operation(); // For debugger } // USCI_A0 interrupt service routine #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector=USCI_A2_VECTOR __interrupt void USCI_A2_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(USCI_A2_VECTOR))) USCI_A2_ISR (void) #else #error Compiler not supported! #endif { P5OUT ^= 0x01; switch (__even_in_range(UCA2IV, 2)) { case USCI_NONE: break; // No interrupt case USCI_UART_UCRXIFG: // RXIFG while (!(UCA2IFG & UCTXIFG)) ; // USCI_A2 TX buffer ready? UCA2TXBUF = UCA2RXBUF; // TX -> RXed character break; case USCI_UART_UCTXIFG: break; // TXIFG case USCI_UART_UCSTTIFG: break; // TTIFG case USCI_UART_UCTXCPTIFG: break; // TXCPTIFG default: break; } } // Timer1 interrupt service routine #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector=TIMER1_A0_VECTOR __interrupt void TIMER1_A0_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(TIMER1_A0_VECTOR))) TIMER1_A0_ISR (void) #else #error Compiler not supported! #endif { P5OUT ^= BIT0; // Toggle P1.0 TA1CCR0 += 65535; // Add Offset to CCR0 }
示波器测试LED的频率使一个2Hz的脉冲。也就是说一秒钟中断了4次。
按照缺省SMCLK=1MHz, 定时器应该中断16次,差了这个正4倍。 确实和波特率差4倍对上了。
我Debug,启动外部32768LXT1语句都是过了的。
不知为何SMCLK不是1M,而是256K.
请忙我看看。