This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
UCTXIFG is automatically
reset if a character is written to UCxTXBUF.
就是说向发送寄存器送字节后,UCXIFG会自动清零.
为什么我第一次写入后,没有自动清零呢?还是1.
用的LAUNCHPAD仿真看到的...
UCA0CTLW0 |= UCSWRST; // **Put state machine in reset**
UCA0CTLW0 |= UCMST+UCSYNC+UCCKPL+UCMSB+UCSSEL_3; // 3-pin, 8-bit SPI master Clock polarity high, MSB , SMCLK=DCO
UCA0BR0 = 0x02; // /2 baud
UCA0BR1 = 0; //
UCA0MCTLW = 0; // No modulation
UCA0STATW|=UCLISTEN; //Receive the transmitted;
UCA0CTLW0 &= ~UCSWRST; // **Initialize USCI state machine**
//UCA0IE |= UCTXIE; // Enable USCI_A0 TX interrupt We will use no interruption.
P1SEL1 |= BIT5;
P2SEL1 |= BIT0 + BIT1;
void spiw(unsigned char word)
{
while((UCA0IFG&UCTXIFG)==0);
UCA0TXBUF=word;
};
执行到这,写入第一个...但UCTIFG没有自动请0..
UCB0CTLW0 |= UCSWRST; // **Put state machine in reset**
UCB0CTLW0 &= ~UCCKPH;
UCB0CTLW0 |= UCMST+UCSYNC+UCMSB; // 3-pin, 8-bit SPI master // Clock polarity high, MSB
UCB0CTLW0 |= UCSSEL_2; // SMCLK
UCB0BR0 = 0x08; // /2
UCB0BR1 = 0; //
UCB0CTLW0 &= ~UCSWRST; // **Initialize USCI state machine**
UCB0IFG &= ~(UCRXIFG+UCTXIFG);
for(i=0;i<ucByteCnt;i++)
{
UCB0TXBUF =ucData[i];
while (!(UCB0IFG&UCTXIFG)); // USCI_B0 TX buffer ready?
while (!(UCB0IFG&UCRXIFG)); // USCI_B0 TX buffer ready?
ucData[i]=UCB0RXBUF;
}
请参考已经能够使用的代码
33.3.8.1 SPI Transmit Interrupt Operation
The UCTXIFG interrupt flag is set by the transmitter to indicate that UCxTXBUF is ready to accept another character. An interrupt request is generated if UCTXIE and GIE are also set. UCTXIFG is automatically reset if a character is written to UCxTXBUF.
UCTXIFG is set after a PUC or when UCSWRST = 1. UCTXIE is reset after a PUC or when UCSWRST = 1.
所以要记得清零操作,也就是UCB0IFG &= ~(UCRXIFG+UCTXIFG);