Other Parts Discussed in Thread: MSP430FR6972
芯片型号:MSP430FR6972
问题:我想要的结果是一次转换信号,转换两个通道,然后不通过中断读取这两个值,但是每次完成转换后通道14的值都不准(为0xFFF,但这个值根据我的程序这个时候采的电压不应该是这个值,我量过),后来我加了一个for循环,发现下一次采集到的数据是对的,连试几次也是这样。根本就不是我预想的。是我哪里理解错了吗?
相关代码:
static void For_Real_Sample(void)
{
ADC_CAP_BAT_Init();
while(REFCTL0 & REFGENBUSY); // If ref generator busy, WAIT
REFCTL0 |= REFVSEL_2 | REFON; // Select internal ref = 2.5V
// Internal Reference ON
ADC12CTL0 &= ~ADC12ENC;
ADC12CTL0 = ADC12ON | ADC12SHT0_4 | ADC12MSC; // Turn on ADC12, set sampling time 64 ADC12CLK,采样保持时间尽量长
ADC12CTL1 = ADC12SHP |ADC12SHS_0 | ADC12CONSEQ_1 | ADC12SSEL_3 | ADC12PDIV_1; // ADC12SC触发采样,序列通道采样 0-1,SMCLK/4
ADC12CTL3 = ADC12CSTARTADD2;
ADC12MCTL2 = ADC12INCH_12 | ADC12VRSEL_1; //ADC_CAP
ADC12MCTL3 = ADC12INCH_14 | ADC12VRSEL_1 | ADC12EOS; //ADC_BAT
ADC12IER0 = 0; //关闭中断
while(!(REFCTL0 & REFGENRDY)); // Wait for reference generator
// to settle
// ADC12CTL0 |= ADC12ENC;
}
//读取转换的两个通道值
void Read_ADC(void)
{
if((indicator->WorkStatus == LowPower))
{
For_Real_Sample();
for(i=0; i<5; i++)
{
ADC12CTL0 |= ADC12ENC | ADC12SC;
while(ADC12IFGR0 & ADC12IFG3 == 0);
temp = ADC12MEM2;
// temp_s = temp * 5000/4096; //单位mv
// indicator->Voltage_Cap = temp_s;
temp = ADC12MEM3;
// temp_s = temp * 5000/4096; //单位mv
// indicator->Voltage_Bat = temp_s;
}
ADC_CAP_BAT_DeInit();
Stop_ADC();
}
}