This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5992勘误表中PMM31类似问题

大家好

         最近一直被430的重启问题所困扰,出现的概率虽然比较低,但是设备运行过程中时不时的重启还是给设备的可靠性以及检测增加了不确定性,希望碰到类似问题的朋友或者官方的人员能够给一个好的解决方案。

       a. 设备要是保证实时采样,采样频率在4.1K,40ms计算一次,采样通过定时器进行触发,采集两个通道的数据;

       b. 设备在采样期间会进入低功耗LPM2,这样能够降低设备功耗,设备需要长期运行,因此对功耗比较在意;

       c. 设备需要射频433通讯,射频通讯会触发外部中断;

       d. 设备在应用过程中,会出现死机的问题,由于存在硬件看门狗,会进行重启,但是重启比较明显,如果设备在检测过程中出现问题,很可能会漏掉一些重要的测量数据,对设备的功能与性能方面产生影响。

      通过勘误表发现PMM31问题与我当前碰到的问题比较相似,类似于LPM2模式切换中碰到AD采样引起的异常,但是设备采样中如果不进入LPM2,对设备的功耗影响较大,希望大家给一些意见或方法,帮忙分析问题也行,谢谢。