This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MSP 430X41X 要液晶显示时一定要接32.768K 晶振么? 内部DCO 可以单独用吗
32768不是必须的,至于为什么一般都接32768,原因有以下:
1. 带断码LCD的,一般都会与时间显示有关系,所以32768用来做RTC;
2. 如果考虑低功耗应用,外部32768是不错的选择;
这是我能想到的两个方面,如果你没有此类需求,可以直接用内部DCO。
你好,不是一定的,段码LCD显示需要不断刷新,MSP430F41x 的 LCD 刷新时钟来自于 Basic Timer,所以只需要有时钟供给 BT 就可以,不一定要是32.768KHz。