This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F672X中的引脚VASYS,VDSYS,DVSYS到底起什么作用?



VASYS,VDSYS,DVSYS按照DATASHEET刚开始我的理解跟Vcore差不多,是提供做测试用,便于知道内部模拟电压和数字电压,但多看了几次又感觉不太像,外面要接指定的电容,VDSYS和DVSYS还要连接,不知道为什么?难道芯片里面不会连接好吗?请高手指点下!!

  • VASYS 是芯片内模拟电路的电源,VDSYS是芯片内数字电路(除GPIO)的电源,DVSYS是GPIO的电源.

    一般处于EMC的考虑芯片的模拟电源和数字电源会分开提供,不过很少看到GPIO和数字电路分开供电的。我想可能设计者最初的想法是想让GPIO支持更广的电压范围,所以GPIO电源单独提供。

  • VASYS和VDSYS以及DVSYS是向芯片内部提供电源吗?如果是,那AVCC和DVCC不是已经提供了模拟和数字电路的电源了吗?

  • MSP430F672X/MSP430F673X layout guide lines

    Guide lines:

    1, VCORE is for internal use only. No external current loading is possible. VCORE should only be connected to the CVCORE Recommended capacitor at VCORE 470 nF.

    Vcore pin 外接滤波电容必须为470nF。

    2, LCDCAP/R33 must be connected to DVSS if not used.

    LCDCAP/R33 pin 如果没有使用,必须接到DVSS。

    3, The pins VDSYS and DVSYS must be connected externally on board for proper device operation.

    VDSYS、DVSYS pin外部连接在一起。

    4,  It is recommended to power AVCC and DVCC from the same source. A maximum difference of 0.3 V between V(AVCC) and V(DVCC) can be tolerated during power up and operation.

    AVCC,DVCC使用同一个电压源供电。在上电和工作的时候,AVCC 和 DVCC电压压差不应超过0.3V。

    5, Recommended capacitor at pins DVCC, AVCC, AUX1, AUX2 is 4.7 μF

        DVCC, AVCC, AUX1, AUX2 pin 推荐电源退耦合/滤波电容为4.7uF。

       Recommended capacitor at pins VDSYS and VASYS is 4.7 μF

       VDSYS、VASYS推荐推荐电源退耦合/滤波电容为4.7uF。

       Recommended capacitor at pin AUX3 0.47 μF

       AUX3推荐推荐推荐电源退耦合/滤波电容为0.47uF。

    6, VREF pin 滤波电容尽可能就近引脚放置。