我用的是CCSV5编程的,在配置USICNT时无法对它写入值,不知道这是为什么?而且无法跳出中断,我猜应该是因为USIIFG无法自动清零的原因吧。
下面是我的代码:
//SPI初始化程序
void SPI_INIT(void)
{
//P1SEL |= BIT5 + BIT6 + BIT7 ;
USICTL0 |= USIPE7 + USIPE6 + USIPE5 + USIMST + USIOE; // Port, SPI master
USICTL1 |= USIIE; // Counter interrupt, flag remains set
USICKCTL = USIDIV_1 + USISSEL_2; // /2 SMCLK
USICTL0 &= ~USISWRST; // USI released for operation
P1DIR |= BIT0 + BIT1 + BIT2;
//P1DIR |= 0x01; // Reset Slave
//P1DIR &= ~0x01;
USISRL = 0x46;
delay_us(300);
USICNT |= USICNT2 + USICNT1; // re-load counter
//USIIFG = 0; // init-load counter
//USICTL1 &= ~USIIFG;
}
uchar SPI_RW(uchar byte)
{
delay_ms(1);
while ((USIIFG & USICTL1)); // Counter clear?
USISRL = byte;
// USICNT = 8; // re-load counter
delay_us(200);
return USISRL;
}
// USI interrupt service routine
#pragma vector=USI_VECTOR
__interrupt void universal_serial_interface(void)
{
// USISRL = *SPI_Data ;
//USICNT |= BIT2; // re-load counter
//USIFG = 0;
USICNT |= USICNT2 + USICNT1;
//USICTL1 &= ~USIIFG;
}