This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5962IPNR

MSP430FR5962IPNR型号在程序运行过程使用空的flash进行数据存储,每次写入数据到flash MCU就重启,不能写入数据到flash,请帮忙提供参考代码或者相关说明文档

  • 看例程

    //******************************************************************************
    //   MSP430FR59xx Demo - Long word writes to FRAM
    //
    //   Description: Use long word write to write to 512 byte blocks of FRAM.
    //   Toggle LED after every 100 writes.
    //   NOTE: Running this example for extended periods will impact the FRAM
    //   endurance. MPU is also enabled by default in CCS.
    //   MCLK = SMCLK = default DCO
    //
    //           MSP430FR5969
    //         ---------------
    //     /|\|               |
    //      | |               |
    //      --|RST            |
    //        |               |
    //        |               |
    //        |          P1.0 |---> LED
    //
    //   Kathryn Adamsky
    //   Texas Instruments Inc.
    //   July 2016 (Updated) | August 2012 (Created)
    //   Built with IAR Embedded Workbench V5.40 & Code Composer Studio V5.5
    //******************************************************************************
    #include <msp430.h>
    
    #define WRITE_SIZE 128                           
    
    void FRAMWrite(void);
    
    unsigned char count = 0;
    unsigned long data;
    
    #if defined(__TI_COMPILER_VERSION__)
    #pragma PERSISTENT(FRAM_write)
    unsigned long FRAM_write[WRITE_SIZE] = {0};
    #elif defined(__IAR_SYSTEMS_ICC__)
    __persistent unsigned long FRAM_write[WRITE_SIZE] = {0};
    #elif defined(__GNUC__)
    unsigned long __attribute__((persistent)) FRAM_write[WRITE_SIZE] = {0};
    #else
    #error Compiler not supported!
    #endif
    
    int main(void)
    {
      WDTCTL = WDTPW | WDTHOLD;                 // Stop WDT
    
      // Configure GPIO
      P1OUT &= ~BIT0;                           // Clear P1.0 output latch for a defined power-on state
      P1DIR |= BIT0;                            // Set P1.0 to output direction
    
      // Disable the GPIO power-on default high-impedance mode to activate
      // previously configured port settings
      PM5CTL0 &= ~LOCKLPM5;
    

  • 您可以在MSPWARE内查找例程

    C:\ti\msp\MSP430Ware_3_80_07_00\examples\devices\MSP430FR5xx_6xx\MSP430FR599x_MSP430FR596x_Code_Examples