使用了IAR自带的MSP430F5xx_6xx串口例程,我用的串口是UA2的所以改了相关部分,但是问题多多
1.下载完程序后串口输出1,给串口发送数据过半天返回一个0,再发数据就能快速返回了。
2.当不发送数据后,串口会不断自动输出0,速度很慢
代码如下:
/* --COPYRIGHT--,BSD
* Copyright (c) 2016, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
* --/COPYRIGHT--*/
//******************************************************************************
//! This example shows how to configure the UART module as the loopback to
//! verify that received data is sent data.
//!
//! MSP430F5438A
//! -----------------
//! RST -| P3.4/UCA0TXD|----|
//! | | |
//! | | |
//! | P3.5/UCA0RXD|----|
//! | |
//!
//!
//! This example uses the following peripherals and I/O signals. You must
//! review these and change as needed for your own board:
//! - UART peripheral
//! - GPIO Port peripheral (for UART pins)
//! - UCA0TXD
//! - UCA0RXD
//!
//! This example uses the following interrupt handlers. To use this example
//! in your own application you must add these interrupt handlers to your
//! vector table.
//! - USCI_A0_VECTOR.
//******************************************************************************
#include "driverlib.h"
//*****************************************************************************
//
//Select Baud rate
//
//*****************************************************************************
#define BAUD_RATE 9600
//*****************************************************************************
//
//Initialize received data
//
//*****************************************************************************
uint8_t receivedData = 0x00;
//*****************************************************************************
//
//Initialize trasnmit data
//
//*****************************************************************************
uint8_t transmitData = 0x00;
uint8_t check = 0;
void main(void)
{
//Stop WDT
WDT_A_hold(WDT_A_BASE);
//P3.4,5 = USCI_A0 TXD/RXD
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_P9,
GPIO_PIN4 + GPIO_PIN5
);
//Baudrate = 9600, clock freq = 1.048MHz
//UCBRx = 109, UCBRFx = 0, UCBRSx = 2, UCOS16 = 0
USCI_A_UART_initParam param = {0};
param.selectClockSource = USCI_A_UART_CLOCKSOURCE_SMCLK;
param.clockPrescalar = 109;
param.firstModReg = 0;
param.secondModReg = 2;
param.parity = USCI_A_UART_NO_PARITY;
param.msborLsbFirst = USCI_A_UART_LSB_FIRST;
param.numberofStopBits = USCI_A_UART_ONE_STOP_BIT;
param.uartMode = USCI_A_UART_MODE;
param.overSampling = USCI_A_UART_LOW_FREQUENCY_BAUDRATE_GENERATION;
if(STATUS_FAIL == USCI_A_UART_init(USCI_A2_BASE, ¶m))
{
return;
}
//Enable UART module for operation
USCI_A_UART_enable(USCI_A2_BASE);
//Enable Receive Interrupt
USCI_A_UART_clearInterrupt(USCI_A2_BASE,
USCI_A_UART_RECEIVE_INTERRUPT);
USCI_A_UART_enableInterrupt(USCI_A2_BASE,
USCI_A_UART_RECEIVE_INTERRUPT);
__enable_interrupt();
while(1)
{
transmitData = transmitData + 1; // Increment TX data
// Load data onto buffer
USCI_A_UART_transmitData(USCI_A2_BASE,
transmitData);
while(check != 1)
{
;
}
check = 0;
}
}
//******************************************************************************
//
//This is the USCI_A0 interrupt vector service routine.
//
//******************************************************************************
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A2_VECTOR
__interrupt
#elif defined(__GNUC__)
__attribute__((interrupt(USCI_A2_VECTOR)))
#endif
void USCI_A2_ISR(void)
{
switch(__even_in_range(UCA2IV,4))
{
//Vector 2 - RXIFG
case 2:
receivedData = USCI_A_UART_receiveData(USCI_A2_BASE);
// if(!(receivedData == transmitData)) // Check value
// {
// while(1)
// {
// ;
// }
// }
check = 1;
break;
default: break;
}
}