请问Ubuntu下做基于430的TinyOS网络需要的硬件平台有哪些?
我用msp5418+CC2500+利尔达usb仿真器可以吗?如果可以需要怎样和linux环境连接起来?如果不可以,需要准备什么硬件?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想对于Tinyos这种小的OS开发的话,其实没有必要使用ubuntu这样的linux操作系统。原因我觉得主要是目前你能找到可使用的交叉编译很少,开发环境,驱动,硬件支持情况都是很大的问题。毕竟不像ARM这种跑linux内核的这种操作系统资源很多。完全可以在IAR或者CCS上进行TinyOS的开发。包括在MSP430上实现UCOSII这样的操作系统都已经在IAR或者CCS实现了开发。
1.需要找到利尔达usb仿真器在linux下的驱动才行,或者使用Sourceforge提供的MSP430 DEBUGGER(详见mspdebug.sourceforge.net),其他硬件够了
2.如果操作系统可以用Window,最好就在OS中装一个Cygwin,MSP430 GCC工具在sourceforge.net/.../index.php,然后用Eclipse工具链整合起来用,这样会方便一点,但是搭建整个开发系统的工作量是较大的,不如直接用IAR或者CCS的评估版先试试。