This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5XX 库 时钟配置问题



在使用MSP430F5XX的库,发现定时器demo中没有系统时钟的初始化代码,上来就是配置定时器的参数,这是怎么回事?

void main(void)
{
    //Stop WDT
    WDT_A_hold(WDT_A_BASE);

    //Set P1.0 to output direction
    GPIO_setAsOutputPin(
        GPIO_PORT_P1,
        GPIO_PIN0
        );

    //Start timer in continuous mode sourced by ACLK
    Timer_A_clearTimerInterrupt(TIMER_A1_BASE);

    Timer_A_initContinuousModeParam param = {0};
    param.clockSource = TIMER_A_CLOCKSOURCE_ACLK;
    param.clockSourceDivider = TIMER_A_CLOCKSOURCE_DIVIDER_1;
    param.timerInterruptEnable_TAIE = TIMER_A_TAIE_INTERRUPT_ENABLE;
    param.timerClear = TIMER_A_DO_CLEAR;
    param.startTimer = true;
    Timer_A_initContinuousMode(TIMER_A1_BASE, &param);

    //Enter LPM0, enable interrupts
    __bis_SR_register(LPM0_bits + GIE);

    //For debugger
    __no_operation();
}

  • 这个例程里定时器使用的是ACLK,ACLK默认上电时开启的,例程里也没有涉及到其他的ACLK的频率,所以不需要初始化。

    如果使用其他时钟或不是默认的频率,要注意先配置时钟。

  • 您可以看一下ucs.h内的说明

    //! This function initializes each of the clock signals. The user must ensure
    //! that this function is called for each clock signal. If not, the default
    //! state is assumed for the particular clock signal. Refer MSP430Ware
    //! documentation for UCS module or Device Family User's Guide for details of
    //! default clock signal states.

    //*****************************************************************************
    //
    //! \brief Initializes a clock signal
    //!
    //! This function initializes each of the clock signals. The user must ensure
    //! that this function is called for each clock signal. If not, the default
    //! state is assumed for the particular clock signal. Refer MSP430Ware
    //! documentation for UCS module or Device Family User's Guide for details of
    //! default clock signal states.
    //!
    //! \param selectedClockSignal selected clock signal
    //!        Valid values are:
    //!        - \b UCS_ACLK
    //!        - \b UCS_MCLK
    //!        - \b UCS_SMCLK
    //!        - \b UCS_FLLREF
    //! \param clockSource is clock source for the selectedClockSignal
    //!        Valid values are:
    //!        - \b UCS_XT1CLK_SELECT
    //!        - \b UCS_VLOCLK_SELECT
    //!        - \b UCS_REFOCLK_SELECT
    //!        - \b UCS_DCOCLK_SELECT
    //!        - \b UCS_DCOCLKDIV_SELECT
    //!        - \b UCS_XT2CLK_SELECT
    //! \param clockSourceDivider selected the clock divider to calculate
    //!        clocksignal from clock source.
    //!        Valid values are:
    //!        - \b UCS_CLOCK_DIVIDER_1 [Default]
    //!        - \b UCS_CLOCK_DIVIDER_2
    //!        - \b UCS_CLOCK_DIVIDER_4
    //!        - \b UCS_CLOCK_DIVIDER_8
    //!        - \b UCS_CLOCK_DIVIDER_12 - [Valid only for UCS_FLLREF]
    //!        - \b UCS_CLOCK_DIVIDER_16
    //!        - \b UCS_CLOCK_DIVIDER_32 - [Not valid for UCS_FLLREF]
    //!
    //! Modified bits of \b UCSCTL5 register, bits of \b UCSCTL4 register and bits
    //! of \b UCSCTL3 register.
    //!
    //! \return None
    //
    //*****************************************************************************
    extern void UCS_initClockSignal(uint8_t selectedClockSignal,
                                    uint16_t clockSource,
                                    uint16_t clockSourceDivider);

  • 嗯明白了,另外定时器参数 compareOutputMode是什么意思?我不想有任何外部输出,选择bit就可以了吗?
  • uint16_t compareOutputMode;

    //! Is the count to be compared with in compare mode
  • 我指的是这个,默认的bitValue是啥含义?

    //! - \b TIMER_A_OUTPUTMODE_OUTBITVALUE [Default]
        //! - \b TIMER_A_OUTPUTMODE_SET
        //! - \b TIMER_A_OUTPUTMODE_TOGGLE_RESET
        //! - \b TIMER_A_OUTPUTMODE_SET_RESET
        //! - \b TIMER_A_OUTPUTMODE_TOGGLE
        //! - \b TIMER_A_OUTPUTMODE_RESET
        //! - \b TIMER_A_OUTPUTMODE_TOGGLE_SET
        //! - \b TIMER_A_OUTPUTMODE_RESET_SET
        uint16_t compareOutputMode;

  • TIMER_A_OUTPUTMODE_OUTBITVALUE 表示 输出由TACCTLx的OUT位直接控制
  • 建议楼主先找个msp430f5的教程看一下,然后再对照数据手册看例程,就很容易理解了。

    http://bbs.21ic.com/icview-584664-1-1.html