This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5438A ADC采样配置问题



想用ADC单通道轮询方式采集电压,但有几个疑问:

1.有扩展模式和脉冲模式 ,该选哪个?

2.tsync时间是多长?

3.如何确定采样时间的长度?

4.单通道轮询采集,每次采集是不是都要进行开始转换操作?

  • ADC单通道轮询方式采集?你说的是单通道多次采样方式吗?

    这几个问题基本都要根据实际的应用场合来选择。

    1、重复采样一般用脉冲模式ADC12SHP = 1 

    4、adc每次的采样,包括信号采样和转换两个过程。

  • 采样保持分两种模式,由ADC12CTL1的ADC12SHP位控制,ADC12SHP=0时是扩展模式,ADC12SHP=1时是脉冲模式。

    1 扩展模式,SHI信号上升沿开始采样,上升沿后的高电平时间即为采样时间,SHI信号下降沿进行采样结果转换,转换需要13个ADC12CLK。

    2 脉冲模式,SHI信号触发采样定时器,采样定时器就是控制什么时候开始采样,什么时候开始转换,采样定时器由ADC12CTL0的ADC12SHT0和

    ADC12SHT1配置,在采样定时器时间内进行采样,采样后就立即进行采样结果转换。

    3 转换时间在脉冲采样模式和扩展采样模式都是相同的。
  • tsync同步时间是多长呢?
  • 您可以看一下www.ti.com/.../slau208q.pdf

    Figure 28-4. Extended Sample Mode

    Figure 28-5. Pulse Sample Mode

    半个clk左右,这个时间一般是比较固定的