This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

定时器对串口输出的影响

MCU用F5438A,在UCSI_UART例程中加了定时器中断,不开不要紧,开了串口打印几十个字符就停止了,这是怎么回事?

附代码:

/* --COPYRIGHT--,BSD
 * Copyright (c) 2016, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 * --/COPYRIGHT--*/
//******************************************************************************
//! This example shows how to configure the UART module as the loopback to
//! verify that received data is sent data.
//!
//!               MSP430F5438A
//!             -----------------
//!       RST -|     P3.4/UCA0TXD|----|
//!            |                 |    |
//!            |                 |    |
//!            |     P3.5/UCA0RXD|----|
//!            |                 |
//!
//!
//! This example uses the following peripherals and I/O signals.  You must
//! review these and change as needed for your own board:
//! - UART peripheral
//! - GPIO Port peripheral (for UART pins)
//! - UCA0TXD
//! - UCA0RXD
//!
//! This example uses the following interrupt handlers.  To use this example
//! in your own application you must add these interrupt handlers to your
//! vector table.
//! - USCI_A0_VECTOR.
//******************************************************************************
#include "driverlib.h"
#include <RingBuf.h>
//*****************************************************************************
//
//Select Baud rate
//
//*****************************************************************************
#define BAUD_RATE                               9600
//*****************************************************************************
//
//Initialize received data
//
//*****************************************************************************
volatile uint8_t receivedData = 0xAA;
//*****************************************************************************
//
//Initialize trasnmit data
//
//*****************************************************************************
uint8_t transmitData = 0x00;

uint8_t check = 0;

volatile uint16_t timer_count = 0;
uint16_t timeout = 5; //��ʱ5ms
uint8_t rxbuf[128] = {0};
volatile uint8_t state = 0x00;
uint8_t txbuf[128] = {1};
RingBuf_Object uart1;
RingBuf_Handle handle = &uart1;
    
void main(void)
{
    //Stop WDT
    WDT_A_hold(WDT_A_BASE);
    
    
    
    RingBuf_construct(handle, (uint8_t*)rxbuf, 128);
    
    //P3.4,5 = USCI_A0 TXD/RXD
    GPIO_setAsPeripheralModuleFunctionInputPin(
        GPIO_PORT_P9,
        GPIO_PIN4 + GPIO_PIN5
        );

    //Baudrate = 9600, clock freq = 1.048MHz
    //UCBRx = 109, UCBRFx = 0, UCBRSx = 2, UCOS16 = 0
    USCI_A_UART_initParam param = {0};
    param.selectClockSource = USCI_A_UART_CLOCKSOURCE_SMCLK;
    param.clockPrescalar = 109;
    param.firstModReg = 0;
    param.secondModReg = 2;
    param.parity = USCI_A_UART_NO_PARITY;
    param.msborLsbFirst = USCI_A_UART_LSB_FIRST;
    param.numberofStopBits = USCI_A_UART_ONE_STOP_BIT;
    param.uartMode = USCI_A_UART_MODE;
    param.overSampling = USCI_A_UART_LOW_FREQUENCY_BAUDRATE_GENERATION;

    if(STATUS_FAIL == USCI_A_UART_init(USCI_A2_BASE, &param))
    {
        return;
    }

    //Enable UART module for operation
    USCI_A_UART_enable(USCI_A2_BASE);

    //Enable Receive Interrupt
    USCI_A_UART_clearInterrupt(USCI_A2_BASE,
                               USCI_A_UART_RECEIVE_INTERRUPT);
    USCI_A_UART_enableInterrupt(USCI_A2_BASE,
                                USCI_A_UART_RECEIVE_INTERRUPT);
    
    
    //Start timer in continuous mode sourced by SMCLK
    Timer_A_initContinuousModeParam initContParam = {0};
    initContParam.clockSource = TIMER_A_CLOCKSOURCE_SMCLK;
    initContParam.clockSourceDivider = TIMER_A_CLOCKSOURCE_DIVIDER_1;
    initContParam.timerInterruptEnable_TAIE = TIMER_A_TAIE_INTERRUPT_ENABLE;
    initContParam.timerClear = TIMER_A_DO_CLEAR;
    initContParam.startTimer = false;
    Timer_A_initContinuousMode(TIMER_A1_BASE, &initContParam);

    //Initiaze compare mode
    Timer_A_clearCaptureCompareInterrupt(TIMER_A1_BASE,
                                         TIMER_A_CAPTURECOMPARE_REGISTER_0
                                         );

    Timer_A_initCompareModeParam initCompParam = {0};
    initCompParam.compareRegister = TIMER_A_CAPTURECOMPARE_REGISTER_0;
    initCompParam.compareInterruptEnable =
        TIMER_A_CAPTURECOMPARE_INTERRUPT_DISABLE;
    initCompParam.compareOutputMode = TIMER_A_OUTPUTMODE_OUTBITVALUE;
    initCompParam.compareValue = 5000;
    Timer_A_initCompareMode(TIMER_A1_BASE, &initCompParam);

    Timer_A_startCounter(TIMER_A1_BASE,
                         TIMER_A_CONTINUOUS_MODE
                         );
  __bis_SR_register(GIE);
    //__enable_interrupt();

    while(1)
    {
//      if(timer_count > timeout)
//      { 
//        if(state == 1)
//        {
//          state = 0;
//          
//          uint8_t num = RingBuf_getCount(handle);
//          for(uint8_t i = 0; i<num;i++)
//          {
//            RingBuf_get(handle, &txbuf[i]);
//            USCI_A_UART_transmitData(USCI_A2_BASE,txbuf[i]);
//          }
//          
//        } 
//        else
//        {
//          timer_count = 0; 
//        }
//      }
       USCI_A_UART_transmitData(USCI_A2_BASE,timer_count);
    }
}

//******************************************************************************
//
//This is the USCI_A0 interrupt vector service routine.
//
//******************************************************************************
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A2_VECTOR
__interrupt
#elif defined(__GNUC__)
__attribute__((interrupt(USCI_A2_VECTOR)))
#endif
void USCI_A0_ISR(void)
{
    switch(__even_in_range(UCA2IV,4))
    {
    //Vector 2 - RXIFG
    case 2:
        receivedData = USCI_A_UART_receiveData(USCI_A2_BASE);
        RingBuf_put(handle, receivedData);
        timer_count = 0;
        state = 1;
        break;
    default: break;
    }
}


//******************************************************************************
//
//This is the TIMER1_A3 interrupt vector service routine.
//
//******************************************************************************
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=TIMER1_A0_VECTOR
__interrupt
#elif defined(__GNUC__)
__attribute__((interrupt(TIMER1_A0_VECTOR)))
#endif
void TIMER1_A0_ISR(void)
{
  switch(__even_in_range(TA0IV,0x0E))
    {
    //Vector 2 - RXIFG
    case 0x0E:
      timer_count ++; //���ϼ���
    default: break;
    }
}

  • 很抱歉,我现在无法拿板子测试。您现在每次串口打印的十几个字符是固定的吗?您为何要加定时器中断?
  • 问题解决了,是例程的问题 TA1用了TA0的中断向量。另外还有些小问题:
    1.在配置串口引脚时,为什么都用了GPIO_setAsPeripheralModuleFunctionInputPin函数,没用outputpin呢?
    有官方资料说F5系列不支持outputpin,但有的例程中却又使用了输出API,这怎么说?
    2.PMM_setVCore(PMM_CORE_LEVEL_1); LEVEL1-3哪个是最高的等级?