This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430 i2041 温度计算?sd24



sd24采样温度,应该如何计算转换为温度。

我得到的原始值是460W。应该如何换算为温度。文档上面没看明白。

电压计算文档还是描述的很清楚

  • www.ti.com.cn/.../slac676f.zip
    参考下上面这个代码示例,MSP430i20xx 代码示例,解压路径下slac676f\MSP430i20xx_Code_Examples\C\msp430i20xx_sd24_06就是温度计算的例程。
    或者参考下下面这个文档的13.2.11章节,有个计算公式的。
    www.ti.com.cn/.../slau335.pdf
  • 谢谢楼上的回答

    我直接贴一下例程代码吧,该例程转换完成后,将结果存储在变量中,然后转换为摄氏度和华氏度值。

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2013, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     * 
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //  MSP430i20xx Demo - SD24, Using the Integrated Temperature Sensor
    //
    //  Description: This program uses the SD24 module to perform a single
    //  conversion on a single channel which is internally connected to the SD24's
    //  temperature sensor. Once the conversion is completed, the result is stored in
    //  a variable then converted into Celsius and Fahrenheit values.
    //
    //  Test by setting a breakpoint at the indicated line. Upon reaching the breakpoint
    //  the conversion result will be stored in the results array. The result will
    //  then be taken and converted into degrees K, C, and F and be saved in the same
    //  array.
    //
    //  ACLK = 32kHz, MCLK = SMCLK = Calibrated DCO = 16.384MHz, SD_CLK = 1.024MHz
    //  * Ensure low_level_init.c is included when building/running this example *
    //
    //  Notes: For minimum Vcc required for SD24 module - see datasheet
    //         100nF cap btw Vref and AVss is recommended when using 1.2V ref
    //
    //  Sensor's temperature coefficient is 2.158mV/K (from datasheet)
    //  Sensor's offset voltage ranges from -100mv to 100mV (assume 0)
    //  Vsensor = 1.32mV * DegK + Vsensor_offset (assuming 0mv for offset)
    //  Vsensor = (SD24MEM0)/32767 * Vref(mV)
    //  DegK = (SD24MEM0 * 1200)/32767/2.158 = (SD24MEM0 * 1200)/70711
    //  DegC =  DegK - 273
    //  DegF = (DegC * 9/5) + 32
    //
    //
    //               MSP430i20xx
    //             -----------------
    //         /|\|                |
    //          | |                |
    //          --|RST             |
    //            |                |        (A0.6+/- connected internally)
    //            |A0.6+      VREF |---+    (to SD24's temperature sensor)
    //            |A0.6-           |   |
    //            |                |  -+- 100nF
    //            |                |  -+-
    //            |                |   |
    //            |           AVss |---+
    //
    //  T. Witt
    //  Texas Instruments, Inc
    //  September 2013
    //  Built with Code Composer Studio v5.5
    //******************************************************************************
    #include "msp430.h"
    
    unsigned int  results[4];                       // SD24 Conversion and Temp Results
                                                    // results[0] = raw SD24 results
                                                    // results[1] = temp in K
                                                    // results[2] = temp in C
                                                    // results[3] = temp in F
    
    void main(void) {
        WDTCTL = WDTPW | WDTHOLD;                   // Stop WDT
    
        SD24CTL = SD24REFS;                         // Internal ref
        SD24CCTL0  |= SD24SNGL | SD24DF | SD24IE;   // Enable interrupt
        SD24INCTL0 |= SD24INCH_6;                   // Internal temp sensor
    
        __delay_cycles(3200);                       // Delay ~200us for 1.2V ref to settle
    
        while(1) {
            SD24CCTL0 |= SD24SC;                    // Set bit to start conversion
            __bis_SR_register(LPM0_bits | GIE);     // Enter LPM0 w/ interrupts
            __no_operation();                       // For debugger
    
            // Calculate Temperatures in different scales
            results[1] = ((unsigned long)results[0] * 1200)/70711;
            results[2] = results[1] - 273;
            results[3] = (results[2] * 9/5) + 32;
    
            __no_operation();                       // SET BREAKPOINT HERE
        }
    }
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=SD24_VECTOR
    __interrupt void SD24_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(SD24_VECTOR))) SD24_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
        switch (__even_in_range(SD24IV,SD24IV_SD24MEM3)) {
            case SD24IV_NONE: break;
            case SD24IV_SD24OVIFG: break;
            case SD24IV_SD24MEM0:
                       results[0] = SD24MEM0;       // Save CH0 results (clears IFG)
                       break;
            case SD24IV_SD24MEM1: break;
            case SD24IV_SD24MEM2: break;
            case SD24IV_SD24MEM3: break;
            default: break;
        }
        __bic_SR_register_on_exit(LPM0_bits);       // Wake up from LPM0
    }