Other Parts Discussed in Thread: MSP430G2231
各位大神,你好!
本来是一个刚接触MSP430G的菜鸟,现在我用ADC10进行ADC采集,但是进不了ADC中断,跪求指导,谢谢了!代码如下:
void main(void)
{
long IntDeg=0;
long temp=0;
WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
//配置时钟
BCSCTL3 = LFXT1S_2; //低高频选OLV,并作为ACLK时钟源
BCSCTL2 = SELM_3 + DIVM_0; //MCLK时钟源选VLO(或LFXT1),MCLK不分频
IFG1 &= ~OFIFG; //清时钟失效中断标志
_BIS_SR(SCG0 + SCG1 + OSCOFF); //关DCO、SMCLK、LFXT1等
BuzzerInit();
//timer0_init();
ADC10_init();
while(1)
{
//LPM3;
ADC10CTL0 |= ENC + ADC10SC; // Sampling and conversion start
_EINT();
//_bis_SR_register(CPUOFF + GIE); // LPM0 with interrupts enabled
//LPM3;
//-----ADC转换完成中断唤醒CPU后才执行以下代码-----
temp = ADC10MEM; //读取AD采样值
IntDeg= (temp*3.3)/1024;
__no_operation(); // SET BREAKPOINT HERE
}
}
void ADC10_init(void)
{
ADC10CTL0 &= ~ENC;
P1SEL=0xFF;//将io口选择为AD输入
P1DIR &= ~BIT1;
ADC10AE0 |= BIT1; // P1.1 ADC option select
//ADC10CTL0 = ADC10IE + ADC10ON + REFON + ADC10SHT_3 + SREF_1;
//ADC10CTL1 = CONSEQ_0 + ADC10SSEL_1 + ADC10DIV_0 + SHS_0 + INCH_1;
ADC10CTL0 = ADC10SR + ADC10ON + ADC10IE; //启动ADC,开中断
ADC10CTL1 = INCH_0 + ADC10SSEL_1 + CONSEQ_0; //ADC时钟为ACLK, 单通道单次模式
ADC10CTL0 |= ENC;
}
#pragma vector=ADC10_VECTOR
__interrupt void ADC10_ISR_HOOK(void)
{
P1OUT^=BIT6;
//_bic_SR_register_on_exit(LPM4_bits);
//LPM3_EXIT;
}
无法进入这个中断ADC10_ISR_HOOK,求指导!