This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430f149 通过timerA 产生的PWM控制外围电路电压并AD采集,但是采集不到数据



程序如下:

uint TT=1600;
void Init_TimerA(void)
{
  TACCR0=2000-1;                  // 脉宽                  
  TACCR2=TT;                   
TACCTL2=OUTMOD_7;         //设CCR2输出单元为复位/置位输出模式
  TACTL=TASSEL_2+ID_3+MC_1+TACLR; //子系统时钟+8分频+增计数模式+计数器器清零
}
void bujin(void)                        //间隔3秒PWM占空比改变
{
    TT=TT-64;
    Init_TimerA();
    start_ADC12();                    //AD采集电压
    delay_bujin(1);                    //延时3秒
    while(TT>1200)
    {
      TT=TT-64;
      Init_TimerA();     
     start_ADC12();                   //AD采集电压
      delay_bujin(1);
    }
    if(TT<1200)
    {
      TT=TT+64;
      Init_TimerA();
      start_ADC12();                  //AD采集电压
      delay_bujin(1);
      while(TT<1840)
      {
        TT=TT+64;
        Init_TimerA();
        start_ADC12();                  //AD采集电压 
        delay_bujin(1);
      }
    }
   
}