Other Parts Discussed in Thread: CC430F6137
您好
请问CC430 ADC使用内部参考电压 数值不正常,ADC 值维持300多,不随着电压变化。
使用内部参考电压有何要求?
1 目前的设计P2.4(VREF-)悬空,
手册上这么说的,悬空是不是不行呀?
Negative terminal for the ADC reference voltage for both sources, the internal reference
voltage, or an external applied reference voltage (CC430F613x only
2 代码是参考官方例程,内部参考
REFCTL0 |= REFMSTR+REFVSEL_2+REFON+REFTCOFF;
/* Initialize ADC12 */
ADC12CTL0 = ADC12ON+ADC12SHT02; // Turn on ADC12, set sampling time
ADC12CTL1 = ADC12SHP; // Use sampling timer
ADC12MCTL0 = ADC12SREF_1; // Vr+=Vref+ and Vr-=AVss
__delay_cycles(75); // 75 us delay @ ~1MHz
ADC12CTL0 |= ADC12ENC;