This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BT-MSPAUDSOURCE Tools Bluetooth and MSP430 Audio开发板(MSP430F5229)只能打印输出乱码?

大家好:

    我们购买了BT-MSPAUDSOURCE Tools Bluetooth and MSP430 Audio开发板(MSP430F5229),现在连接P4.5(PM_UCA1RXD)P4.4(PM_UCA1TXD)以及地线;通过USB-TTL的转换器与PC串口相连, 现在只能输出乱码!

     请问我们应该接哪个口(地线), 现所有的波特率都试过了, 只能输出乱码!该怎么解决?

  • 请您详细说明下您的问题。您现在是使用的TI哪个例程还是您自己的程序?
  • 您好:
    我们使用的类似A3DPDemo_SNK(以它为基础改写),现在的状况如下:
    1). 利用手机可以探测到设备:MSP-SNK-19E3E6设备
    2). 使用3套不同的USB-TTL设备(例如:PL-2303HX为主芯片),接TX,RX和地线(例如:P3 COAXIAL TEST PORT的2A)
    均输出乱码!
  • 请您看一下

    processors.wiki.ti.com/.../CC256x_Audio_Source_User_Guide

    的开箱即用实验(能否正常运行?)

    Step 4: Connect the board to PC
    Connect J15 connector (Rx & Tx) with a UART-2-USB cable to get access to the MSP430's UART, A Virtual Serial Port (COM x) under Ports (COM & LPT) will be enumerated . Attach a Terminal program like Tera Term to the serial port x for the board. The serial parameters to use are 9600 Baud, 8,n,1 and no flow control. Once connected, reset the device using Reset button and you should see the stack getting initialized on the terminal
  • 谢谢!
    我们连接P4.5(J15 的1 /PM_UCA1RXD)和UART-2-USB cable,
    请问:1). 应该用USB-TTL呢?还是USB-RS232?
    2). 应该接开发板的那个"地接口"呢?
  • 我重新看了一下发现P4.5 已经被原始demo使用了,做log 使用以及配置使用了。所以您现在无法使用P4.5

    processors.wiki.ti.com/.../CC256x_TI_Bluetooth_Stack_AssistedA2DPSinkDemo_App
  • Susan 您好:
    谢谢!
    我们借助的就是A3DPDemo_SNK,利用P4.5+P4.4+GND(DNI的2A); 结果蓝牙设备“MSP-SNK-01F5B3”已经被识别出来!
    但串口"USB-SERIAL CH340 (COM8)“只能输出乱码!
    该怎么解决?
    (是需要如下改变:
    1). 更改GND的端口, 从DNI的2A---->?
    2). 更改USB转接头,从USB-TTL---->USB-SERIAL?
    3). ......
    )
  • 1、建议先看一下 CH340和开发板是否共地了

    2、检查串口助手的波特率等参数配置和开发板程序里是否一致