Other Parts Discussed in Thread: MSP430F5229
大家好:
我们购买了BT-MSPAUDSOURCE Tools Bluetooth and MSP430 Audio开发板(MSP430F5229),希望提供中断处理程序(最好主设备,从属设备各一套);最好完整一些(宏定义,初始化,执行完整部分)
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F5229
大家好:
我们购买了BT-MSPAUDSOURCE Tools Bluetooth and MSP430 Audio开发板(MSP430F5229),希望提供中断处理程序(最好主设备,从属设备各一套);最好完整一些(宏定义,初始化,执行完整部分)
谢谢!
SuSan, 您好:
按照“蓝牙传输”的理论, 我们希望蓝牙主设备采用“广播方式”发出数据包;蓝牙从设备接收到数据,产生中断,解析数据包内容,进行相应处理!
我们使用的MSP430F5229芯片(开发板是:BT-MSPAUDSOURCE Tools Bluetooth and MSP430 Audio开发板),我们希望以它为基础的
大家好:
您看如下的MSP430的蓝牙接收中断处理程序,改装时注意几项?
MSP430 的 UART 例程您可以参考
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430F552x Demo - USCI_A0, Ultra-Low Pwr UART 2400 Echo ISR, 32kHz ACLK
//
// Description: Echo a received character, RX ISR used. Normal mode is LPM3,
// USCI_A0 RX interrupt triggers TX Echo.
// ACLK = REFO = ~32768Hz, MCLK = SMCLK = DCO ~1.045MHz
// Baud rate divider with 32768Hz XTAL @2400 -- from User's Guide
// See User Guide for baud rate divider table
//
// MSP430F552x
// -----------------
// /|\| |
// | | |
// --|RST |
// | |
// | P3.3/UCA0TXD|------------>
// | | 2400 - 8N1
// | P3.4/UCA0RXD|<------------
//
// Bhargavi Nisarga
// Texas Instruments Inc.
// April 2009
// Built with CCSv4 and IAR Embedded Workbench Version: 4.21
//******************************************************************************
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
P3SEL = BIT3+BIT4; // P3.4,5 = USCI_A0 TXD/RXD
UCA0CTL1 |= UCSWRST; // **Put state machine in reset**
UCA0CTL1 |= UCSSEL_1; // CLK = ACLK
UCA0BR0 = 0x0D; // 2400 (see User's Guide)
UCA0BR1 = 0x00; //
UCA0MCTL |= UCBRS_6+UCBRF_0; // Modulation UCBRSx=6, UCBRFx=0
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
UCA0IE |= UCRXIE; // Enable USCI_A1 RX interrupt
__bis_SR_register(LPM3_bits + GIE); // Enter LPM3, interrupts enabled
__no_operation(); // For debugger
}
// Echo back RXed character, confirm TX buffer is ready first
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCA0IV,4))
{
case 0:break; // Vector 0 - no interrupt
case 2: // Vector 2 - RXIFG
while (!(UCA0IFG&UCTXIFG)); // USCI_A1 TX buffer ready?
UCA0TXBUF = UCA0RXBUF; // TX -> RXed character
break;
case 4:break; // Vector 4 - TXIFG
default: break;
}
}
大家好:
经过“理论“确认,USCI_A0_VECTOR(HCI_RX_1V8_CC---->MSP430F5229的37管脚:P3.3/UCA0TXD)正是我们蓝牙的主接收端口!
但我们将这个中断处理程序写入后, (
请参考:
// Echo back RXed character, confirm TX buffer is ready first #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector=USCI_A0_VECTOR __interrupt void USCI_A0_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void) #else #error Compiler not supported! #endif { switch(__even_in_range(UCA0IV,4)) { case 0:break; // Vector 0 - no interrupt case 2: // Vector 2 - RXIFG while (!(UCA0IFG&UCTXIFG)); // USCI_A1 TX buffer ready? UCA0TXBUF = UCA0RXBUF; // TX -> RXed character break; case 4:break; // Vector 4 - TXIFG default: break; } })
程序下载后就跑飞了, 不能跳转到main()入口处!
如何破解?
dirtwillfly, 您好:
我认同您关于工程设置的假设,它的报错信息:
“Verify error at address 0xfff0 on target 0x92 in file 0x84
Verify error at address 0xfff0, Value should be 0x84 but is 0x92.
Failed to load debugee: F:\ti\.....\Exe\A3DPDemo_SNK.d43”