程序和Debug就是这样。新手求指教
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
//*******************************************************************************
// MSP430x26x Demo - Software Toggle P1.0
//
// Description: Toggle P1.0 by xor'ing P1.0 inside of a software loop.
// ACLK= n/a, MCLK= SMCLK= default DCO ~1.045MHz
//
// MSP430F261x/241x
// -----------------
// /|\| XIN|-
// | | |
// --|RST XOUT|-
// | |
// | P1.0|-->LED
//
// B. Nisarga
// Texas Instruments Inc.
// September 2007
// Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.42A
//******************************************************************************
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer
P1DIR |= 0x01; // Set P1.0 to output direction
for (;;)
{
volatile unsigned int i;
P1OUT ^= 0x01; // Toggle P1.0 using exclusive-OR
i = 50000; // Delay
do (i--);
while (i != 0);
}
}