This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【TI 测评】+MSP-EXP432P401R 小黑板下载那些事

Other Parts Discussed in Thread: UNIFLASH

经过几天的折腾,终于把MSP-EXP432P401R的下载搞定了,把经验给大家分享下。

首先是板载XDS110-ET的firmware的版本,一定要是Rev 1.0的,千万不要升级,升级完后降级是很困难的。

MDK检测到的 Rev1.2  XDS110-ET的信息如下所示:

其次是下载的方式,可以通过CCS(这个只能debug间接下载,无法直接下载)、MDK、IAR、UNIFLASH、DSLite(一个批处理下载文件)这些方式下载。

首先是CCS的下载,CCS软件的版本一定不要用最新的,最新的CCS软件是RevB版本的芯片的。而且用最新的CCS会自动更新固件,更新后的XDS110-ET固件会变为Rev1.2 的版本,下载的提示如下所示:

这个时候怎么办呢?换CCS的版本,换CCS8以下的版本,我这里换的是CCS7.4的版本,使用XDS110-ET  Rev1.2 和XDS110-ET  Rev1.0的版本都是可以下载的。debug运行界面如下所示:

注意:如果用XDS110-ET  Rev1.2 第一次用CCS7.4给板子下载,会给XDS110-ET降级为Rev1.0的,因为CCS7.4自带的XDS110的固件版本就是Rev1.0的。

           但我插入另一块Rev1.2小黑板,不提示升级了,这个需要找到在哪更新的,或许TI的员工可以来提示下。

 

然后是MDK的下载,MDK的下载有两点需要注意的:

1.仿真下载器需要选择CNSIS-DAP Debugger

2.XDS110-ET 的版本必须是 Rev1.0的,在MDK5.24环境下 Rev1.2版本的固件是不支持下载的。使用Rev1.2下载的报错如下所示:

 

最后要讲的是UNIFLASH的下载,UNIFLASH的下载同样对XDS110-ET的固件版本没要求,但是对UNIFLASH的版本有要求,最新的UNIFLASH5.1的版本是不支持的,我用的是UNIFLASH4.0的版本,UNIFLASH4.0的下载链接如下所示:

http://processors.wiki.ti.com/index.php/Category:CCS_UniFlash_Release_Notes_Archive