This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5994 编译问题 Warning[Pe161]:unrecognized #pragma

您好,我下载了SLAA698的LEA的软件包,用IAR Embedded Workbench for MSP430 IDE 7.10.1 编译其中的一个工程“benchmark_q15-cfft_fixed_512”,出现“Warning[Pe161]:unrecognized #pragma”,应该指的是“#pragma PERSISTENT(inputVector)

int32_t inputVector[SAMPLES] = {”

还出现 Error[e16]: Segment DATA20_Z (size: 0x808 align: 0xb) is too long for segment definition. At least 0x408 more bytes needed. The problem occurred while processing the segment placement command "-Z(DATA)DATA20_I,DATA20_Z,DATA20_N", where at the moment of placement the available memory ranges were "CODE:2400-2bff"

   Reserved ranges relevant to this placement:

   1c00-2bff            DATA20_I

请问这些有什么解决方法?